Skip to main content
Kpodu.1
Associate III
Dec 2, 2020 3:51 PM UTC
Question

option bytes to be set during manufacturing when launching the product to market.

Hi All,

We are launching one of our product to market. And we are using STM32F429ZiT6 MCU.

Recently I am going through the data sheet for list of option bytes which needs to be set during manufacturing. I have an understanding on what should be set. But I just want to confirm my understanding and these will serve the purpose.

Below is our application roughly.

In the first 3 sectors we have the bootloader-------- which never changes

We do an OTA for the application. So the rest of sectors are divided in to 2---1 for main application....1 for back up.

The rest of sectors(4-24) are divided into 2 -----10 sectors each for --- application and back up

so we do write and erase operations from sector 4-24.

So given the above situation.

The option bytes we are setting is

RDP- > Level 2(0xCC) because no one must be able to read through JTAG, SWV,...etc

Write protection on sector 0, sector 1 , sector 2 ------because bootloader is unchanged.

Rest of the sectors are not write protected as we are erasing and writing them.

Above are the option bytes. Any suggestion?

Thanks,

krishna

This topic has been closed for replies.

1 reply

Bowman32
ST Employee
Dec 3, 2020 11:43 AM UTC

Hi @Kpodu.1​ 

Your understanding is correct. However you can refer to RM0090 Rev18 for more details about option bytes.

Bouraoui