Skip to main content
FMaro.1
Associate II
December 3, 2020
Question

What is de CRC16 used on SPI peripheral? the Polynomial is configurable, but the init value and reverse or not, is not documented.

I have a SPI on STM32F746 configured:

/* SPI6 init function */

void MX_SPI6_Init(void)

{

 hspi6.Instance = SPI6;

 hspi6.Init.Mode = SPI_MODE_MASTER;

 hspi6.Init.Direction = SPI_DIRECTION_2LINES;

 hspi6.Init.DataSize = SPI_DATASIZE_16BIT;

 hspi6.Init.CLKPolarity = SPI_POLARITY_LOW;

 hspi6.Init.CLKPhase = SPI_PHASE_2EDGE;

 hspi6.Init.NSS = SPI_NSS_HARD_OUTPUT;

 hspi6.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;

 hspi6.Init.FirstBit = SPI_FIRSTBIT_MSB;

 hspi6.Init.TIMode = SPI_TIMODE_DISABLE;

 hspi6.Init.CRCCalculation = SPI_CRCCALCULATION_ENABLE;

 hspi6.Init.CRCPolynomial = 32773;

 hspi6.Init.CRCLength = SPI_CRC_LENGTH_16BIT;

 hspi6.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;

 if (HAL_SPI_Init(&hspi6) != HAL_OK)

 {

  Error_Handler();

 }

}

void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)

{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

 if(spiHandle->Instance==SPI2)

 {

 /* USER CODE BEGIN SPI2_MspInit 0 */

 /* USER CODE END SPI2_MspInit 0 */

  /* SPI2 clock enable */

  __HAL_RCC_SPI2_CLK_ENABLE();

  __HAL_RCC_GPIOI_CLK_ENABLE();

  /**SPI2 GPIO Configuration

  PI1   ------> SPI2_SCK

  PI2   ------> SPI2_MISO

  PI3   ------> SPI2_MOSI

  */

  GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

  GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;

  HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);

 /* USER CODE BEGIN SPI2_MspInit 1 */

 /* USER CODE END SPI2_MspInit 1 */

 }

 else if(spiHandle->Instance==SPI6)

 {

 /* USER CODE BEGIN SPI6_MspInit 0 */

 /* USER CODE END SPI6_MspInit 0 */

  /* SPI6 clock enable */

  __HAL_RCC_SPI6_CLK_ENABLE();

  __HAL_RCC_GPIOA_CLK_ENABLE();

  __HAL_RCC_GPIOG_CLK_ENABLE();

  /**SPI6 GPIO Configuration

  PA4   ------> SPI6_NSS

  PA5   ------> SPI6_SCK

  PA6   ------> SPI6_MISO

  PG14   ------> SPI6_MOSI

  */

  GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

  GPIO_InitStruct.Alternate = GPIO_AF8_SPI6;

  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = GPIO_PIN_14;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

  GPIO_InitStruct.Alternate = GPIO_AF5_SPI6;

  HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

  /* SPI6 DMA Init */

  /* SPI6_RX Init */

  hdma_spi6_rx.Instance = DMA2_Stream6;

  hdma_spi6_rx.Init.Channel = DMA_CHANNEL_1;

  hdma_spi6_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;

  hdma_spi6_rx.Init.PeriphInc = DMA_PINC_DISABLE;

  hdma_spi6_rx.Init.MemInc = DMA_MINC_ENABLE;

  hdma_spi6_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;

  hdma_spi6_rx.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;

  hdma_spi6_rx.Init.Mode = DMA_NORMAL;

  hdma_spi6_rx.Init.Priority = DMA_PRIORITY_LOW;

  hdma_spi6_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

  if (HAL_DMA_Init(&hdma_spi6_rx) != HAL_OK)

  {

   Error_Handler();

  }

  __HAL_LINKDMA(spiHandle,hdmarx,hdma_spi6_rx);

  /* SPI6_TX Init */

  hdma_spi6_tx.Instance = DMA2_Stream5;

  hdma_spi6_tx.Init.Channel = DMA_CHANNEL_1;

  hdma_spi6_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;

  hdma_spi6_tx.Init.PeriphInc = DMA_PINC_DISABLE;

  hdma_spi6_tx.Init.MemInc = DMA_MINC_ENABLE;

  hdma_spi6_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;

  hdma_spi6_tx.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;

  hdma_spi6_tx.Init.Mode = DMA_NORMAL;

  hdma_spi6_tx.Init.Priority = DMA_PRIORITY_LOW;

  hdma_spi6_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

  if (HAL_DMA_Init(&hdma_spi6_tx) != HAL_OK)

  {

   Error_Handler();

  }

  __HAL_LINKDMA(spiHandle,hdmatx,hdma_spi6_tx);

 /* USER CODE BEGIN SPI6_MspInit 1 */

 /* USER CODE END SPI6_MspInit 1 */

 }

}

This topic has been closed for replies.

1 reply

TDK
December 3, 2020

https://community.st.com/s/question/0D50X00009XkfZPSAZ/unable-to-understand-how-the-crc-calculation-is-done-in-the-spi-module

Link in the post seems to be broken, but the code is there to give you the answers you're looking for.

"If you feel a post has answered your question, please click ""Accept as Solution""."