[Solved] Clarification on total usable PWM channels Posted on October 09, 2014 at 21:29I am trying to maximize the number of unique 16-bit PWM outputs that I can use simultaneously on the SPC560P40L1CEFAR (64 pins). I have gathered the following information from the specification, and some of it appears to be conflicting.1 Flex PWM unit8 complementary or independent channels4 PWM submodulesPWMX pin can optionally output a third PWM signal from each submoduleI count 10 PWM output channels though: A0, A1 A2, B0, B1, B2, B3, X0, X1, X2; B2 and X2 are both only available on pin 52Which output channels correspond to which submodules? And which channels cannot produce unique PWM signals?I also noticed a paradox on page 24 of the SPC560P (34L and 40L) specification. On the same page it says: Channels not used for PWM generation can be used for input capture functions.A few lines down it then says: Capture capability for PWMA, PWMB, an