Skip to main content
marcohartung9
Associate
Jul 2, 2014 2:29 PM UTC
Solved

CR95HF tuning Timer Window and Receiver Gain

Posted on July 02, 2014 at 16:29

Hello

I want to build a reader to communicate with ISO14443A and ISO15693 tags using the CR95HF transceiver IC. I build a 2 turn PCB antenna and calculated the matching of the PCB antenna according to AN4327 and the excel tool.

With VPS_TX = 3,3V I get performance equal to the PLUG_CR95HF demo board.

I tried also to match the antenna for VPS_TX = 5V (assuming better read range) and with this setup it is possible to power tags over a greater distance but I cannot communicate (receive) with the tags. I get little improvement by tweaking the Timer Window and Receiver Gain (5.8.1 and 5.8.2 CR95HF datasheet). But the only way to determine these values I found was �try and see�.

So my question is how to measure or determine the right values for these parameters.

With best regards

Marco

#cr95hf #cr95hf #5v
This topic has been closed for replies.
Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Aug 28, 2014 2:39 PM UTC
Posted on August 28, 2014 at 16:39

Hello,

Is the AN3433 helping?

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00034250.pdf

Have a nice day,

ST NFC RFID  Dynamic tag support

1 reply

Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
Aug 28, 2014 2:39 PM UTC
Posted on August 28, 2014 at 16:39

Hello,

Is the AN3433 helping?

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00034250.pdf

Have a nice day,

ST NFC RFID  Dynamic tag support