Skip to main content
davidt.jones-19
Associate
Oct 9, 2014 7:29 PM UTC
Solved

[Solved] Clarification on total usable PWM channels

Posted on October 09, 2014 at 21:29

I am trying to maximize the number of unique 16-bit PWM outputs that I can use simultaneously on the SPC560P40L1CEFAR (64 pins).  I have gathered the following information from the specification, and some of it appears to be conflicting.

1 Flex PWM unit

8 complementary or independent channels

4 PWM submodules

PWMX pin can optionally output a third PWM signal from each submodule

I count 10 PWM output channels though:

    A0, A1 A2, B0, B1, B2, B3, X0, X1, X2;

    B2 and X2 are both only available on pin 52

Which output channels correspond to which submodules?  And which channels cannot produce unique PWM signals?

I also noticed a paradox on page 24 of the SPC560P (34L and 40L) specification.  On the same page it says:

    Channels not used for PWM generation can be used for input capture functions.

A few lines down it then says:

    Capture capability for PWMA, PWMB, and PWMX channels not supported

Does this mean I need to use timer pins for input capture instead of the PWM pins?

#pwm #spc56
This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Nov 24, 2014 1:25 PM UTC
Posted on November 24, 2014 at 14:25

Hello David ,

Here is an answer from a PWM Expert

sorry for the late answer

''The FlexPWM doesn’t support input capture function, on the datasheet there is a wrong information. In order to perform input capture you should use eTimer as you mentioned.

INFO:

Sub-mod 0: PA0, PB0,PX0

Sub-mod 1: PA1, PB1,PX1

Sub-mod 2: PA2, PB2,PX2

Sub-mod 3: PA3, PB3,PX3  -  On 64pins PA3 and PX3 are not available

PB0 (not PB2) and PX2 are both only available on pin 52…so you can use only 9 PWM signals simultaneously…''

           Best Regards

                                Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Nov 24, 2014 1:25 PM UTC
Posted on November 24, 2014 at 14:25

Hello David ,

Here is an answer from a PWM Expert

sorry for the late answer

''The FlexPWM doesn’t support input capture function, on the datasheet there is a wrong information. In order to perform input capture you should use eTimer as you mentioned.

INFO:

Sub-mod 0: PA0, PB0,PX0

Sub-mod 1: PA1, PB1,PX1

Sub-mod 2: PA2, PB2,PX2

Sub-mod 3: PA3, PB3,PX3  -  On 64pins PA3 and PX3 are not available

PB0 (not PB2) and PX2 are both only available on pin 52…so you can use only 9 PWM signals simultaneously…''

           Best Regards

                                Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
davidt.jones-19
Associate
Nov 24, 2014 7:33 PM UTC
Posted on November 24, 2014 at 20:33

Thank you for the reply.  I chose to scale down number of channels to be safe, but this confirms my conservative assumptions.