Skip to main content
sja
Associate
Sep 23, 2014 1:46 PM UTC
Solved

SPC5-UDESTK Serial Console ?

Posted on September 23, 2014 at 15:46

I am using UDE 4.2.05 with the SPC560B-DIS (which has UDE debug hardware built in)

I can load and run code via JTAG but ...

How do I access the serial port connection to the target device ???

The target microcontroller UART is connected to the FTDI USB/serial/JTAG device but

I do not see a COM port show up on the PC for the target USB/serial connection.

Should this show up as a COM port or perhaps in a UDE window ??

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Sep 24, 2014 8:59 AM UTC
    Posted on September 24, 2014 at 10:59

    Hello Adams ,

    you can find in attachment a document how to install the driver :

    Best regards

    Erwan

    ________________

    Attachments :

    FTDI_Installation_driver_on_SPC560X_Discovery_board_cx369645_1.0_D2.docx : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Sb&d=%2Fa%2F0X0000000bZB%2FGShbxE0szlE8Amb7z3DQ1Ritv2kaXV0g8YUUrwBAm1E&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Sep 23, 2014 3:01 PM UTC
    Posted on September 23, 2014 at 17:01

    Hello Adams ,

    Take the driver inside PLS Tools

    c:\Program Files (x86)\pls\UDE 4.2\Driver\JtagUsbDriver\

    and

    enable VCP in Device Manager(cf screenshot) for each driver

    after rebooting the device .. you should see the COM PORT in your device manager

    By default , the console UART is set to 38400 bauds.

    Best regards

    Erwan

    ________________

    Attachments :

    2014-09-23_165614.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Sq&d=%2Fa%2F0X0000000bZC%2FZARwjO0UqHHwcSOhAh4V.z3Jistg2BuTZlp9Up8A1P4&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Sep 24, 2014 8:59 AM UTC
    Posted on September 24, 2014 at 10:59

    Hello Adams ,

    you can find in attachment a document how to install the driver :

    Best regards

    Erwan

    ________________

    Attachments :

    FTDI_Installation_driver_on_SPC560X_Discovery_board_cx369645_1.0_D2.docx : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Sb&d=%2Fa%2F0X0000000bZB%2FGShbxE0szlE8Amb7z3DQ1Ritv2kaXV0g8YUUrwBAm1E&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.