How stringent are the limits on the "General Operating Conditions"? Hello,I am using a STM32H745ZI in a project and have USART1 configured as a UART. I updated STM32CubeMX to version 6.2.0 today and the clock page is telling me that "USART1,6 clock source frequency must be <= 75 MHz", as per image attached.Earlier versions have not given me this error.I know, I can ignore the error and generate the code anyway.The only place where I think this can come from is as follows. I am using VOS2, and in the device specific datasheet DS12923, table 23 on page 111 says that the maximum APB clock frequency in VOS2 is 75 MHz.Firstly, I think this is a bug in CubeMX because RM0399 states on page 2197 that "There is no constraint between usart_pclk and usart_ker_ck: usart_ker_ck can be faster or slower than usart_pclk. The only limitation is the software ability to manage the communication fast enough.". I cannot find any documentation that says USART1 kernel clock must be limited to 75 MHz.Secondly it got me wondering, how stringent that table is to a maximum li