Skip to main content
Pasi MYLLYMAKI
ST Employee
Mar 3, 2021 4:20 PM UTC
Solved

Do you have also another real life example for FSM in sensors? Is the interval data split the only application? Any others apps?

..

    This topic has been closed for replies.
    Carlo LARGHI
    Carlo LARGHIBest answer
    Visitor II
    Mar 3, 2021 5:28 PM UTC

    there are many examples, you can refer to Github repository highlighted in webinar material for some. In particular, in the context of the IIS2ICLX, the mentioned application for monitoring the traffic load on a bridge rely on combined usage of FSM and MLC

    The other example showed in the webinar is the direct angle output from inclinometer based on MLC classification. With other ST sensors with MLC, we have also examples of detecting if drilling machine is idle, tightening screw or drilling to wood etc, this type of example could then be extended to automated machinery and this example can be for sure adapted also to run on IIS2ICLX.

    1 reply

    Carlo LARGHI
    Carlo LARGHIBest answer
    Visitor II
    Mar 3, 2021 5:28 PM UTC

    there are many examples, you can refer to Github repository highlighted in webinar material for some. In particular, in the context of the IIS2ICLX, the mentioned application for monitoring the traffic load on a bridge rely on combined usage of FSM and MLC

    The other example showed in the webinar is the direct angle output from inclinometer based on MLC classification. With other ST sensors with MLC, we have also examples of detecting if drilling machine is idle, tightening screw or drilling to wood etc, this type of example could then be extended to automated machinery and this example can be for sure adapted also to run on IIS2ICLX.