Solved
Eleon BORLINIBest answer
ST Employee
Mar 3, 2021 3:18 PM UTC
Hi @Louis Loving ,
I would suggest you to use the IIS2DH Github repository (link) for a check on a MIS2DH-compatible device.
An example of base configuration is the following one (for example for the wake-up interrupt on INT1, iis2dh_wake_up.c:(
/* High-pass filter enabled on interrupt activity 1 */
iis2dh_high_pass_int_conf_set(&dev_ctx, IIS2DH_ON_INT1_GEN);
/* Enable HP filter for wake-up event detection
* Use this setting to remove gravity on data output
*/
iis2dh_high_pass_on_outputs_set(&dev_ctx, PROPERTY_ENABLE);
/* Enable AOI1 on int1 pin */
iis2dh_pin_int1_config_get(&dev_ctx, &ctrl_reg3);
ctrl_reg3.i1_aoi1 = PROPERTY_ENABLE;
iis2dh_pin_int1_config_set(&dev_ctx, &ctrl_reg3);
/* Interrupt 1 pin latched */
iis2dh_int1_pin_notification_mode_set(&dev_ctx, IIS2DH_INT1_LATCHED);
/* Set full scale to 2 g */
iis2dh_full_scale_set(&dev_ctx, IIS2DH_2g);
/* Set interrupt threshold to 0x10 -> 250 mg */
iis2dh_int1_gen_threshold_set(&dev_ctx, 0x10);
/* Set no time duration */
iis2dh_int1_gen_duration_set(&dev_ctx, 0);
/* Dummy read to force the HP filter to current acceleration value. */
iis2dh_filter_reference_get(&dev_ctx, &dummy);
/* Configure wake-up interrupt event on all axis */
iis2dh_int1_gen_conf_get(&dev_ctx, &int1_cfg);
int1_cfg.zhie = PROPERTY_ENABLE;
int1_cfg.yhie = PROPERTY_ENABLE;
int1_cfg.xhie = PROPERTY_ENABLE;
int1_cfg.aoi = PROPERTY_DISABLE;
iis2dh_int1_gen_conf_set(&dev_ctx, &int1_cfg);
/* Set device in HR mode */
iis2dh_operating_mode_set(&dev_ctx, IIS2DH_HR_12bit);
/* Set Output Data Rate to 100 Hz */
iis2dh_data_rate_set(&dev_ctx, IIS2DH_ODR_100Hz);Can you please check if you have correctly configured the sensor?
-Eleon