Skip to main content
HThak.2
Associate
Mar 3, 2021 12:52 PM UTC
Solved

Maximum Safe voltage on GPIO Pin

I am a newbie here. I have purchased a STM32G071 Nucleo-64 development board. I wish to interface it to the 5 volts signal(s). The intended interface pins are PB1, PB3 and PB4. The Absolute Maximum ratings VIN states:-

1) Input voltage on FT_xx pins except FT_c = VDD + 4.0 max

2) Input voltage on FT_c pins = 5.5 max

3) Input voltage on any other pin = 4.0 volts max

My Question: -

What are FT_xx pins and FT_c pins? Its not mandatory to use the pins PB1, PB3 and PB4 as listed above, I can use a suitable alternative.

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
Mar 3, 2021 1:24 PM UTC

These are the internal pin structures.

Please check STM32G071RB datasheet, Table 11, page 41.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

1 reply

Mike_ST
Mike_STBest answer
ST Technical Moderator
Mar 3, 2021 1:24 PM UTC

These are the internal pin structures.

Please check STM32G071RB datasheet, Table 11, page 41.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.