Skip to main content
Gregory Go.
Senior III
May 14, 2021 10:57 AM UTC
Question

STUSB_NVM_ReadWriteUtility_v1.01

NVM memory read/write CLI utility for STUSBxxxx

  • Description:

Command-line interface utility to program the NVM memory of STUSBxxx products.

Thanks to this tool, you can easily automate the process of flashing several devices.

It requires a STM32 Nucleo board which is used as a USB-to-I2C adapter.

Create a configuration file corresponding to your USB-C application settings (by using the GUI), and then easily program the chip with this utility in 1 command line.

  • Compatible with: 

STUSB4500, STUSB4500L, STUSB4700, STUSB4710, STUSB1600, STUSB1602, STUSB1700, STUSB1702, STUSB4761

  • Usage:

NVM_ReadWriteUtility.exe -command read -output NVM_DUMP.txt

NVM_ReadWriteUtility.exe -command write -input NVM_config.txt

  • Download:

Download the program in attachment.

    This topic has been closed for replies.