2019-05-22 6:42 PM
Hi, I noticed this feature from Bluetooth 5.1.
https://www.bluetooth.com/blog/new-aoa-aod-bluetooth-capabilities/
"The new Bluetooth direction finding feature supports two methods for determining the direction of a Bluetooth signal, both of which are based on the use of an antenna array: angle of arrival (AoA) and angle of departure (AoD)."
I have recently purchased the P-NUCLEO-WB55 from Digikey
https://www.digikey.com/product-detail/en/stmicroelectronics/P-NUCLEO-WB55/497-18384-ND/9857029
and downloaded the STM32WB CubeMX codes.
However, although STM32WB supports Bluetooth 5, I couldn't find codes related to AOA or AOD.
Are there AOA/AOD examples available for P-NUCLEO-WB55?
Thanks.
2021-04-10 1:16 AM
It seems, ST has not much interest in supporting their STM32WB for BLE. I am also looking for answers for similar questions in STM32WB community forum and no success yet. I may wait for some more time and if there no support from ST then I may switch to nRF5340 for Nordic has decent support in their community forums.
2021-04-13 6:57 AM
Hi ST, can you please answer to Matthew’s original question please?
2021-04-21 12:32 AM
This feature requires an antenna array to be supported, the Nucleo board does not support it as there is only one antenna. So I don't expect any example code in the WB FW package.