cancel
Showing results for 
Search instead for 
Did you mean: 

End of Life for STPC Atlas?

jalonso1
Associate II
Posted on October 25, 2005 at 11:11

End of Life for STPC Atlas?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
jalonso1
Associate II
Posted on October 14, 2005 at 07:13

Hello everybody.

I have noticed that STPC Atlas is not RoHS Compliant yet, while there are two STPC Vega versions which are already lead-free.

Does anybody know if ST plans to offer a RoHS Compliant version of STPC Atlas?

Not being so, I suppose it means its End of Life is quite near...

Thank you anyway.

Bye.

balaji_softproff
Associate II
Posted on October 15, 2005 at 06:57

dear sir,

we have built our own board using stpc atlas. If ur sure about end of atlas please notify because we have to shift to other processor (vega).

And can u say what is RoHS?

thank you

Balaji

jalonso1
Associate II
Posted on October 17, 2005 at 13:50

Dear Balaji,

RoHS means Restriction of Hazardous Substances and regulates the use of six ecologically harmful substances. The RoHS European directive states that from the 1st of July 2006, new electrical and electronic equipment put on the market shall not contain lead, mercury, cadmium, hexavalent chromium and two brominated flame retardants (PBB and PBDE).

There are already two STPC Vega versions RoHS compliant, but there is none STPC Atlas Version RoHS compliant. Usually that means the obsolescence of the product is near...

Best regards,

Jose Carlos

kaouther
Associate II
Posted on October 25, 2005 at 08:02

At the first let me clarify that NO END OF LIFE of ATLAS!

STPC Atlas, Lead Free salestypes (E) are available.

Order entry in leadfree is openned.

Thanks.

jalonso1
Associate II
Posted on October 25, 2005 at 11:11

Thanks a lot for such a clarification.