2007-05-30 2:43 AM
Flash ST10F272 with ST10 Flasher tool
2007-05-30 2:35 AM
Hello to all,
I am currently using a ST10F269 and began porting/adapting SW to a ST10F272Z. And now I have some problems to flash my ST10F272. When I open the ST10 Flasher tool (Version 2.3C) the tool trys to load the monitor and I get the following error-message: *LOAD MONITOR-->ERROR Description: InitMonitor failed. Monitor: BSL: No aknowledge Received. Reset your application and reload the monitor. Com: Receive: Timeout or Lost of data The status of the Com Port is always ok and no program occupied the serial interface. And I had also checked the portpins P0L.4 for low signal and P0L.5 for high signal. I think, this is all correct. Can anyone help me to solve my problem? Thanks in advance, Stefan2007-05-30 2:43 AM
Hello Stefan_Mueller,
The ST10Flasher version 2.3C doesn't support the ST10F272. To program the ST10F272, the ST10Flasher version 2.4B should be used. This version is available on the following link: http://www.stmcu.com/modules.php?name=mcu&file=familiesdocs&FAM=17 at the bottom of the web page. You can also refer to the AN2143 ''Programming the ST10F27X embedded Flash using the ST10FLASHER tool'' available also on the same link above. Regards, Najoua. [ This message was edited by: Najoua on 30-05-2007 15:18 ]2017-10-25 12:41 PM
Hello,
I would like to refresh this topic because I'm searching for STFlasher ver 2.4B and I cannot find it. Link above doesn't work for now. Do anybody can support me?
Regards,
Pawel
2018-04-11 8:53 AM
Hi
biuro
,if you are still looking for the ST10FLASHER ver 2.4B, send us a request on
http://www.st.com/content/st_com/en/support/online-support.html
.I just answered to the same request for another customer, and by accident, saw yours pending within our STCommunity.
Might be too late for you, but in case it helps other ST10 users.
Best regards,
Cédric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.