Get ready for the STM32 Summit 2026 | Online, November 3
Join discussions in the Product Forums. Ask questions, learn from your peers, and share insights on ST solutions to accelerate your design journey.
Most recent activity
Hi Team, do ST offer a high-g accelerometer, similar to the LSM6DSV320X on the STEVAL-MKI251A, that supports over 400g with integrated free-fall detection?
I am working on a project in which the sensor data that will calculated by stm32 will be sent via using the esp32 as a wifi module to aws , now the problem is i have inserted the stm32 and esp32 inside a pcb with the required circuit connection but i am having difficulty flashing the code to esp32 or connecting to esp32 , i have tried various methods but cant seem to find a solution. thing is the code cannot be flashed directly to esp32 , it has to be sent via stm32 due to circuit connections and no availability of usb connection ?current status right now:- i am using the process of semihosting to flash the code into stm32 and get results on the serial monitor since i dont have a usb connection for stm32 , i am using the st link of nucleo externally , if someone can help me regarding conversion of my stm32l476 to a bridge to flash code on esp32 or to convert esp32 to wifi module ,it would be very helpful ,this is the last step after this only calibration is required to
Split from Question about ST eSIM solutions - which is solved.This is a new question.Hi!Can you please tell me how the activation process on the ST4SIM-300M chip works now?
Hi! We have two custom boards that we have soldered the ST4SIM-300M eSim to. We have earlier been using the ST4SIM-200M and followed this activiation procedure:https://www.st.com/resource/en/application_note/an5740-st4sim-with-truphone-connectivity--activation-procedure-stmicroelectronics.pdfto get them working with truphone.Now when i try to do the same thing with our new eSim i get the same ICCID from both, this is what i get:at AT%XICCID %XICCID: 89019990001234567893 When i try to enter it on truphones activation page it says that the device is not found.Am i doing something wrong or missing anything?
Hi all,I’m currently working on an Edge AI project using the NUCLEO-N657X0-q and I've run into a roadblock regarding multi-model deployment.I need to run 2 or 3 models on this MCU, scheduled via FreeRTOS. While I can get a single model working fine with STM32Cube.AI Studio, I’m struggling to find a detailed workflow for managing multiple instances.Specific questions:API Naming: How to properly configure Cube.AI to generate unique prefixes for multiple models to avoid link-time conflicts?Memory/Buffer Sharing: Is there a standard way to share a single activation buffer between models to save RAM, given they are called sequentially via FreeRTOS?Task Scheduling: Any known issues or best practices for calling stai_network_run() within a FreeRTOS task? (e.g. stack size or re-entrancy).I’ve checked the ST Edge AI Core docs but couldn't find a concrete example for this multi-model + RTOS use case. If anyone has a reference project or can point me to the right Application Note, I’d really
Hello, I am testing SPI5 TX by GPDMA on an STM32N6 device and I found behavior that seems inconsistent with the reference manual. MCU / Environment MCU: STM32N647X0H Toolchain: STM32CubeIDE 2.1.1 CubeMX / CubeN6 version: STM32Cube_FW_N6_V1.3.0 Issue summaryI configured SPI5 as: Master Simplex TX-only Software NSS SSI set high I configured GPDMA1 Channel0 as: Memory-to-peripheral Source = TX buffer Destination = SPI5->TXDR Transfer length = 8 bytes TX pattern = A5 5A A5 5A A5 5A A5 5A Observed behavior If I write data directly to SPI5->TXDR by CPU, MOSI outputs correctly. If I use GPDMA for SPI5 TX, SCK may appear, but MOSI stays low / no valid TX data is output. I reduced the project to a minimal LL test case and the behavior is reproducible. What I already verified Same SPI5 pin configuration is used in both tests. CPU TX path works with the same SPI configuration. TX buffer content is correct in memory (A5 5A ...). DMA source addres
Hello,According to Table 246 in section 27.3.3 Signal Routing of the STM32U3 Reference Manual, I should be able to configure ADC1_IN6 as an ADC input when using OPAMP1, or ADC1_IN13/ADC2_IN9 when using OPAMP2 such that the output of the opamps are routed internally to the input of the ADC.However, in CubeMX configuration for this device, enabling the Opamp in any capacity "red's out" the option to use the corresponding ADC input for any of these combinations. In this example, OPAMP1 is set to PGA Not Connected, and I am unable to configure the ADC input on IN6.Am I doing something wrong here, or is this simply a bug related to the recent release of this product?Thanks!CubeMX version: 6.17.0OS: Ubuntu 24.04.4Device: STM32U3C5CIUxQ
Hi community.TLV230adc5140 - SAI 4CH(TDM) - STM32 - USB_FS_ 4CHmic - Window(LInux RP5) I reuse partly code from memsmic1 project to create 4 microfone audio device. Everything look well for channel 1 and 2 I got some trouble whit CH3 and CH4. Please help whit wrong channel mapping for channel 3 and 4. It is mapped on channel 1 and 2 on usb interface. One can see it on attached picture. Here is TLV switched off, SAI(DMA call back) reused for 4 sin generator 1,2,3,4 kHz for every supposed channel. Here you see the picture.Where i am wrong?
Hello,I'm working on a project to increase the detection range of the STHS34PF80. During my tests with different LPF and Threshold settings, I noticed that TPRESENCE_L often drops to 0 and stops updating entirely.It feels like the internal algorithm is "absorbing" the signal or the filter is too aggressive.Does changing LPF settings require a specific reset sequence to prevent this?Are there known limitations when trying to push the range beyond 2.2m using software parameters?Any help would be greatly appreciated. Thanks!
Hi everyone, I am working on a dual-core project using the STM32H747XI. I am implementing a custom Tickless Idle mode in FreeRTOS on the Cortex-M7 (CM7) core using LPTIM1 as the wakeup source. I’m facing a specific issue regarding the interaction between D1 and D2 domains: The Scenario: CM4 is running a continuous task (intended to stay active). CM7 enters low-power mode via vPortSuppressTicksAndSleep. If I use HAL_PWR_EnterSLEEPMode(), everything works perfectly—CM4 keeps running, and CM7 wakes up as expected. If I switch to HAL_PWREx_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI, PWR_D1_DOMAIN), the CM4 core seems to "die" or freeze as soon as CM7 enters the DStop state. Is it physically possible for CM4 to continue executing code if the D1 domain is in DStop (CM4 is using only LPTIM1 on D3 and timers on D2)? Code snippet used on CM7: _weak void vPortSuppressTicksAndSleep(TickType_t xExpectedIdleTime) { // Generated when configUSE_TICKLESS_IDLE == 2. // Functio
How to configure the sysTick_Handler(), when we are setting the HCLK 386MHz in CubeMX and systemClock() is generated, but while configuring sysTick(), uint32_t SystemCoreClock = 64000000; already there in system_stm32h7xx_dualcore_boot_cm7_cm4.c(void)SysTick_Config((SystemCoreClock) / 10000);Will it effect mine overall MCU speed and performance, because after all I'm using FMC NAND Flash to communicate with the external Micron Flash, because there I need to calculate the clock cycles need to the write enable (WE), Setup time, Address Latch Enable (ALE) time etc, will be effected, or it is completely independent, should I only consider FMC_CLK which is coming from PLL clock source 2.
Dear sir / madam The UltraLibrarian WBA5M (Module) footprint is flawed. Potentially it can screw the module under reflow.Those center GND pads are not placed correct. I noticed when comparing the ST dev-board module. see image..
Hi all,I noticed that when using the encoder, the motor undergoes an alignment phase during which it completes a rotation until it reaches the position where the Index Z signal is triggered.I was wondering if it's possible to skip this alignment phase by adding the Hall sensors (like with the B-G473E combined with the STEVAL-LVLP01 board), and if so, what should I specify in the Workbench or in the Code?Regards,Jules
I bought STM32F4DISCOVERY. But in the STMcube IDE, i see only STM32F407G-DISC1 board. Are STM32F4DISCOVERY vs STM32F407G-DISC1 same? Can I select STM32F407G-DISC1 and create a project in the IDE and use STM32F4DISCOVERY hardware to run the project? Will it create any issues?
Split from STM32CubeIDE missing “STM32 Project” and CubeMX after fresh installation - that issue was resolved.This is a new issue.The new version 2.1.1 appears pretty useless even after trying to make a project with the separate cubemx. From the IDE you cannot then build the project. It just sits there. I would hope that the IDE is at at capable of building and compiling the project but it appears that is no longer the case.Did you employ someone from microsoft to break it. It was working perfectly before hand. New->STM Project->.....->build->debug. I will revert back to 1.19 to avoid wasting more time and just use an older CubeMX as that was the only reason I upgraded Please leave working software alone or simply improve it and not break it for no reason
I am currently working on an STM32 TrustZone project and trying to implement the following flow:NonSecure world running↓Calls Secure_add()↓Secure world executes↓Returns value 8↓UART prints the result in NonSecure worldHowever, I am facing an issue while jumping from the NonSecure world to the Secure world. The expected secure function execution is not happening properly.If anyone has faced a similar issue or has suggestions regarding NSC gateway configuration, linker settings, or TrustZone function calls, please share your insights. this much i am getting the outCMSE_NS_ENTRY uint32_t Secure_add(uint32_t a, uint32_t b){return a + b;} ------------------------ My Nsc.c entry logic for(int i = 0; i < 5; i++){printf("NONSECURE WORLD RUNNING\r\n");printf("I am amritha\r\n"); //for(volatile int d=0; d<500000; d++);}uint32_t result;printf("Before Secure_add\r\n");result = Secure_add(5,3);printf("Before Secure_add\r\n");printf("Secure result = %lu\r\n",
From Figure 12.STEF033 cannot be used for the case Ilim=1A?Rlimit is valid when the value is more than 120 ohm?
Hi, I'm using a STM32F072's DAC to output a SIN and a COS wave. The problem is I can only output values up to approx. VDDA / 2. The DAC drives unity gain amplifiers to drive a 50 Ohm load. The DAC is connected directly to the amps, using the buffer does not help. VDDA = 3.3 V. Here, CH4 is connected directly to the DAC output via a 10:1 probe. The black things on the scope inputs are 50 Ohm termination, so the CH2 and CH3 signals having only half the amplitude of CH4 is expected. All channels are DC coupled. I'm writing to the DAC using the DHR12L1/2 registers (using the STM32Cube HAL): uint16_t value = (uint16_t) (ltbDacSinLut(ltb_dac_ch1_counter_) ^ 0x8000) & 0xFFF0; HAL_DAC_SetValue(&hdac, DAC_CHANNEL_1, DAC_ALIGN_12B_L, (uint32_t)value);where ltbDacSinLut returns values in the range of [-32768, 32767]. Dividing the value by 2 before writing to the DAC results in undistorted SIN / COS output, but of course the output swing
Hello ST team,I am facing a boot-time crash in OP‑TEE on an STM32MP257DAI3.The system boots through BL2 and BL31 successfully, but OP-TEE triggers a data abort followed by a SERC exception, leading to a panic at <stm32_serc_handle_ilac>.I would appreciate guidance on correct RIF/RISAF configuration for OP-TEE and how to trace SERC exception ID's to actual peripheral .Here is my OPTEE error logWARNING: This OP-TEE configuration might be insecure! WARNING: Embeds insecure stm32mp_provisioning driver ..... I/TC: Platform stm32mp2: flavor PLATFORM_FLAVOR - DT stm32mp257f-ev1.dts I/TC: OP-TEE ST profile: secure_and_system_services D/TC:0 0 call_initcalls:40 level 3 check_ta_store() D/TC:0 0 check_ta_store:418 TA store: "early TA" D/TC:0 0 check_ta_store:418 TA store: "Secure Storage TA" D/TC:0 0 check_ta_store:418 TA store: "REE" D/TC:0 0 call_initcalls:40 level 3 early_ta_init() D/TC:0 0 early_ta_init:56 Early TA 80a4c275-0a47-4905-8285-1486a9771a08 size 46235 (compressed, unco
As the subject states, when I try to run the AI model from the original demo on the STM32N6570-DK board, the screen turns black and the LEDs switch to red.A few days ago, I attempted to run my own AI model. Using STM32CubeProgrammer, I selected the external loader MX25UM1245G_STM32N6570-DK (I believe this may have been incorrect). Then, in the Erasing & Programming section, I uploaded my .bin file, set the start address to 0x70380000, and started the programming process.After that, I tried to debug the STM32N6570-DK Getting Started Object Detection project in STM32CubeIDE. However, I encountered an issue in main.c with the error:#error "PostProcessing type not supported"which persists.Later, I decided to restore the original demo. I erased the external memory using STM32CubeProgrammer,then downloaded the original demo .hex file ("STM32N6570-DK Out-of-the-box demo binary"), and followed the provided instructions.The demo now runs on the board, but when I try to launch the orig
Hello st community!Does anyone managed to get a csi-2 camera working with Nucelo n657 can provide his project as reference, im trying to explore the DCMIPP but I'm getting lost so if any code provided so i can follow along.Thanks!
I am using the STEVAL-MKI238A kit with the LIS2DUX12 chip. This is connected to an NRF52840DK and interfaced using Zephyr's lis2dux12 driver. The eval kit is connected to the SPI3 device using its default settings. I am running an SPI clock of 1Mhz and the VDD and VDIO pins are supplied 1.85V+GND from a shared power supply with the nrf52840dk. The Zephyr lis2dux12 driver is hard coded to use SPI mode 3, so CPOL+CPHA.The lis2dux12 driver fails its INIT sequence by mismatch of the WHO_AM_I readback. The device seemingly returns 0x0C.I have connected a logic analyzer to the pins of the eval kit shows this sequence:- 0x01 is written to register 0x3E to wake the device up from sleep- Once the CS signal is disabled, 50ms passes before the next CS enable to allow the sensor to wake up- A read request is made to register 0x8F (bit 7 read + 0x0F)- The clock idles for 48.5µs before pulsing for the response- The sensor effectively pulses 0000.1100b- However the sensor seems to attempt to set
I notice there is now a github repo with FSM examples; very useful!However, in comparing what I have been successfully using, for example, for shake detection on the LSM6DSV (or LSM6DSV80X) where 30 lines are written to page 0x7A: _i2c_bus->writeByte(i2cAddress, LSM6DSV80X_PAGE_VALUE, 0xC0 | 0x20 | 0x02); // write to CONFIG_A (three thresholds, two masks, two short timers) _i2c_bus->writeByte(i2cAddress, LSM6DSV80X_PAGE_VALUE, 0x00); // write to CONFIG_B _i2c_bus->writeByte(i2cAddress, LSM6DSV80X_PAGE_VALUE, 0x1E); // write to SIZE (30 byte program) _i2c_bus->writeByte(i2cAddress, LSM6DSV80X_PAGE_VALUE, 0x00); // write to SETTINGS _i2c_bus->writeByte(i2cAddress, LSM6DSV80X_PAGE_VALUE, 0x00); // write to RESET POINTER _i2c_bus->writeByte(i2cAddress, LSM6DSV80X_PAGE_VALUE, 0x00); // write to PROGRAM POINTER _i2c_bus->writeByte(i2cAddress, LSM6DSV80X_PAGE_VALUE, 0x66); // write to THRESH1 LSB _i2c_bus->writeByte(i2cAddress, LSM6DSV80X_PAGE_VALUE, 0x3E); // w
Hello,Can anyone tell me how to measure pulse width with the HRTIM? I need to measure a very short pulse from my time domain reflectometer. I am thinking of using the NUCLEO-H753ZI board with the STM32H753ZI MCU. All I know about measuring pulses with the HRTIM is that I need to use the external event registers and that the minimum pulse width must be >2.5 ns. Any help would be greatly appreciated.
Hello everyone!I am trying to get a custom board based on an STM32WBA5MMG to join my existing ZigBee network. As a first test, I have created a basic project in CubeMX, that configures STM32_WPAN to generate a ZigBee project with one OnOff-Endpoint and sets up USART2 for logging. When I generate a CMake-based project and try to compile it in VSCode with the STM32 extensions installed (without making any changes to what CubeMX generated), I get a bunch of linking errors and the build fails:[build] /Users/dg/Library/Application Support/stm32cube/bundles/gnu-tools-for-stm32/14.3.1+st.2/bin/../lib/gcc/arm-none-eabi/14.3.1/../../../../arm-none-eabi/bin/ld: warning: /Users/dg/Library/Application Support/stm32cube/bundles/gnu-tools-for-stm32/14.3.1+st.2/bin/../lib/gcc/arm-none-eabi/14.3.1/thumb/v8-m.main+fp/hard/crtn.o: missing .note.GNU-stack section implies executable stack [build] /Users/dg/Library/Application Support/stm32cube/bundles/gnu-tools-for-stm32/14.3.1+st.2/bin/../lib/gcc/arm-non
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.