Skip to main content
Associate II
Jul 22, 2025 4:13 AM UTC
Solved

STM32U5 + ADS1293: Clean ECG from Lead I, but Noisy/Incorrect Data from Lead II

 

 Trying to Interface ADS1293 with STM32U5 for 3-Lead ECG – Need Help with Lead II Data

Hi STM32 Community :waving_hand:,

We’re trying to build a 3-lead ECG signal acquisition setup using the ADS1293 analog front-end connected via SPI to an STM32U5G9ZJT6Q microcontroller. The goal is to capture and plot Lead I, Lead II, and derive Lead III using TouchGFX.


 What’s Going Well:

  • We are able to receive and plot clean ECG data for Lead I (RA - LA) using CH1 of the ADS1293.

  • SPI communication is stable, and the plotting is handled through TouchGFX without lag.

  • Sampling is working at 500–1000 Hz using a DRDY-based interrupt routine.


What We’re Struggling With:

  • When we try to configure CH2 for Lead II (RA - LL), the data appears noisy, flat, or unstable.

  • We’re using the same initialization and acquisition process for CH2 as we did for CH1, but the result is not usable.

  • For Lead III, we are trying to derive it in software using:

    Lead III=Lead II−Lead I\text{Lead III} = \text{Lead II} - \text{Lead I}Lead III=Lead II−Lead I

    But since Lead II is not clean, Lead III is also affected.


 What We Have Tried:

  • Verified hardware connections and electrode placements – all seem correct.

  • Swapped electrodes to check if the issue is with wiring – no improvement.

  • Checked lead-off detection and ADC status flags – everything seems normal.

  • Confirmed that CH2 is enabled and configured similarly to CH1.

  • SPI read timing and DRDY sync appear to be correct.


 Our Current Register Setup:

#define FLEX_CH1_CN_VALUE 0x11 // INP=IN2 (LA), INN=IN1 (RA) for Lead I

#define FLEX_CH2_CN_VALUE 0x19 // INP=IN3 (LL), INN=IN1 (RA) for Lead II


 Reference:

We’re referring to the ADS1293 datasheet (TI document SLAS969), and focusing particularly on the channel configuration sections starting from page 43:

If anyone wants to verify the register details, please refer to those pages.

 What We’re Looking For:

  1. Has anyone successfully acquired clean Lead II ECG data using ADS1293?

  2. Are there any specific register settings or hardware considerations for CH2 (IN2–IN3) that we might be missing?

  3. Would it be better to acquire only Lead I and Lead II, then derive Lead III entirely in software?

  4. Is there any known issue or errata with CH2 channel configuration on ADS1293?


 System Summary:

  • MCU: STM32U5G9ZJT6Q

  • AFE: ADS1293 (SPI interface)

  • Display: 5” TFT LCD via TouchGFX

  • Electrodes: 3-lead (RA, LA, LL)

  • Sampling: 500–1000 Hz, DRDY interrupt based


We would really appreciate any guidance, working examples, or known-good register maps for this use case. Thank you in advance!

—
Ganesh
Embedded Software Engineer 

Andrew Neil
Andrew NeilBest answer
Super User
Nov 10, 2025 2:27 PM UTC

@JaiGanesh The ADS1293 is a TI part - nothing to do with ST - you need to go to TI for support with their product:

https://www.ti.com/product/ADS1293

https://www.ti.com/product/ADS1293#support-training

 

@Ozone wrote:

I would concentrate on the ADS1293, and experiment with settings and hardware.


Indeed.

The ideal way to do that would be to get the TI ADS1293EVM Evaluation Module - its whole point & purpose is to allow you to experiment & gain familiarity with the ADS1293 on known-good and supported hardware.

 

You certainly need to get the basic data acquisition working first - before worrying about graphics displays and TouchGFX!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

3 replies

Ozone
Principal
Jul 22, 2025 5:30 AM UTC

> When we try to configure CH2 for Lead II (RA - LL), the data appears noisy, flat, or unstable.
> We’re using the same initialization and acquisition process for CH2 as we did for CH1, but the result is not usable.

Your problem is obviously the configuration of the ADS1293, and the signal conditioning hardware.
Especially the ADS1293 seems to be a complex beast.

There is not much you can do on MCU side when the input data are already messed up (GIGO).

I would concentrate on the ADS1293, and experiment with settings and hardware.

Andrew Neil
Andrew NeilBest answer
Super User
Nov 10, 2025 2:27 PM UTC

@JaiGanesh The ADS1293 is a TI part - nothing to do with ST - you need to go to TI for support with their product:

https://www.ti.com/product/ADS1293

https://www.ti.com/product/ADS1293#support-training

 

@Ozone wrote:

I would concentrate on the ADS1293, and experiment with settings and hardware.


Indeed.

The ideal way to do that would be to get the TI ADS1293EVM Evaluation Module - its whole point & purpose is to allow you to experiment & gain familiarity with the ADS1293 on known-good and supported hardware.

 

You certainly need to get the basic data acquisition working first - before worrying about graphics displays and TouchGFX!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Apr 23, 2026 12:20 PM UTC

@Andrew Neil wrote:

you need to go to TI for support with their product


Before doing that, you will need to confirm that your code is correctly following the SPI protocol defined in the TI documentation.

To do that:

  1. Use an oscilloscope to verify that the signals are clean, with good edges, at the correct levels, etc;
  2. Use a logic analyser to verify the SPI activity. 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.