WATCH ON-DEMAND | STM32 Summit 2026
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
Most recent activity
Posted on July 05, 2018 at 21:12Hi,I'm using BlueNRG-MS to transfer data to host PC running windows 10.The connection interval is 15ms, slave latency 5, connection timeout of 300 ms. BlueNRG-MS sends 1 notification of 20 bytes each connection (verified using BLE sniffer). Everything seems to work fine.However, after few seconds of steady link, connection suddenly drops.Running in debug I see that the connection status is '1' and that no disconnection event was received, even tough device is not connected in windows BLE settings.I'm running on 32 MHz and 32 kHz clocks if it matters, HS startup time is calibrated, IFR is configured properly.Any ideas how to solve this?
Posted on July 09, 2018 at 13:01Good day, everyone,I have tried using the ST7590 QFN chip and I found that its functionality is limited, and the TQFP package is the advertised stand-alone chip. I have been advised (if I am going to make a change) I might as well move to the ST8500. If I do make the change I would like to get a feel for the chip first. I have never used an ST microcontroller and I see there is a project building tool called CubeMX. I would like to find out if only the STM32 are supported or are their other chips like the ST8500 are supported?Even though I will need to sign an SLA to use this chip, will I still be able to ask questions in a public forum (such as this one) about setting up UART, analogue-read, digital IO, using the cortex-M4 built-in functions and other such functions or will that breach the contract? I do not intend to put up any documentation I get from signing the SLA, but this is a more complex chip than the ST
Posted on July 09, 2018 at 20:07Looking for someone who is working on asset management with bluetooth mesh, wifi and maybe RFID. we are starting on a new project with asset management and would like to work with someone on this project.
Posted on July 09, 2018 at 16:42I am trying to receive CANopen data (8bytes sent every 1s) with Nucleo L476RG (it has only Master CAN interface but I think it should not matter since CAN is multimaster). For conversion CANH and CANL to CANRx and CANTx I use recommended IC sn65hvd230. In examples I have found only loopback example. If somebody can provide me with a code how to configure CAN for receive periodically mentioned 8 bytes it would be of great help.David#nucleo-l476rg #can
Posted on July 09, 2018 at 11:29What is the supply voltage range for ST485E.The datasheet doesn't give a minimum for the range
Posted on July 01, 2018 at 16:21Hello, I am trying to develop a new product with the SPBTLE-1S module, my idea is to use the module connected to a uC by UART.https://www.st.com/resource/en/datasheet/spbtle-1s.pdf Looking in the datasheet I see that the pinout description changes depending on the 'Mode', but I can't find anywhere how these modes are set.Could anyone help me?I am on the point of defining the hardware connections.Many thanks#spbtle-1s
Posted on July 04, 2018 at 12:44Hello,I am using BluNRG-1 module with Stack v1.0.My clock source is 'LS_SOURCE = LS_SOURCE_INTERNAL_RO', the module has no external oscillator.I used the following code to lower the power consumption, as it is adviced in 'BlueNRG-1 and BlueNRG-2 low power modes.pdf' and I am getting average current consumption about 120 uA.BlueNRG_Sleep(SLEEPMODE_WAKETIMER, WAKEUP_IO13, WAKEUP_IO_LOW, 0);I also tried SLEEPMODE_NOTIMER option with the same current consumption: 120 uA.The advertising interval in my application has been set to 1000 ms.Can you please advice, what setting will make the power consumption below 20 uA?In advance thanks,Evgeny#bluenrg-1 #sleep-mode
Error while parsing Rich Text Content
Posted on May 02, 2018 at 20:11Hello,Where can I find the source code for the Demo Android Apps, such as the 'BlueNRG' app or 'STM32 BLE Profiles' app.Thanks,Ricardo#android-app #bluetooth
Posted on July 01, 2018 at 03:11Hello everyone!! im starting with a proyect that final objective is communicate using sigFox. ok. step by stepi have been all day reading about s2-lp (pcb design, RF bands , etc), i decided buy some dev kit ( STEVAL-FKI868V1) . also buy the s2-lp and the components. i have two questions � what is the IDE to program? � use some usb - spi converter to program directly s2-lp?. any extra suggestion will be a big help. thanks!!.#s2-lp #sigfox #steval-fki868v1
Posted on July 01, 2018 at 10:24Hi.I wanted to buy Bluenrg evaluation board but I couldn't do it because of export restriction.So I designed a board referring to STEVAL-IDB008V1 schematic.Artwork design is very simple so I expected bluenrg to connect with St-link.Sometimes bluenrg was recognized on bluenrg-1 st-link utility but after a short time, VDD and GND became shorted.I think that my soldering skill and circuit design can be a problem. I will re-design my board but I have some question to make sure.Can I program bluenrg with st-link using 4 pins (SWTCK, SWTDIO, RST, GND) ???Is there any cautions or notes for using bluenrg chip?Thank you.#stlink #bluenrg-1 #bluenrg
Posted on June 26, 2018 at 23:21Has anyone else encountered and solved a 'can't halt cpu' issue in IAR EWARM when using the segger j-link to program the BlueNRG-1 part through the 20 pin IDC jtag port on the STEVAL-IDB007V2? If so could you share the fix?I can read and flash the BlueNRG-1 through J-Link commander but that's not a good debug environment. I also have a couple of ST-Link v2s here but those throw errors claiming inability to connect to the CPU. With the J-link IAR's debug log is as follows:Tue Jun 26, 2018 17:10:39: IAR Embedded Workbench 8.20.2 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\bin\armproc.dll) Tue Jun 26, 2018 17:10:40: JLINK command: ProjectFile = C:\Users\hgoldstein\Documents\ST\BlueNRG-1_V1 DK 1.0.0\Project\BLE_Examples\BLE_Chat\EWARM\settings\BLE_Chat_Client.jlink, return = 0 Tue Jun 26, 2018 17:10:40: Device 'BLUENRG1' selected. Tue Jun 26, 2018 17:10:40: Selecting SWD as current target interface. Tue Jun 26, 2018 17:1
Posted on September 07, 2017 at 21:07Hello, I would like to know BlueNRG-1 platform can support UART over BLE? Thank you. EVM Kit: STEVAL-IDB007V1Embedded Software: STSW-BLUENRG1-DKJeffrey#BlueNRG-1#UART over BLE
Posted on June 27, 2018 at 20:31Hi,I have problem with this wifi module.After I saved configuration settings in module (act as wifi client) he does not starts at all.I thought that I destroyed some internal file system structures/module config so I tried to enter into bootloader mode to overwrite firmware and factory settings but without success. It looks like that the module does not response at all.Information about my module:+WIND: Power On (170111-665d284-SPWF01S)I attached boot sequences screen from logic analyzer.Does anyone has idea how to start this module or how to make detail diagnosis of this case?#spwf01sa #wifi-spwf01sa
Posted on June 27, 2018 at 16:46Hi,We're just completing a design based on the ST BlueTooth Low Energy module SPBTLE-RF.However, we are finding it very difficult to find any stock (in the UK at least)SPBTLE-RF is marked as not recommended for new designsSPBTLE-RFTR looks ok and appears to be just a different format (Tape & Reel)But delivery times are anything from 5 weeks to a year !Nucleo development boards for BLE are still featuring this module so I presume it isn't going to be superseded anytime soon ? Thanks for any info anyone may have..#ble #spbtle-rf
Posted on June 25, 2018 at 11:31Hi,I need older version of HAL library for STM32L4.Where can I find it? I need the version 1.7.1.Regards,Piotr#hal #stm32l4-hal #old-versions
Posted on June 27, 2018 at 21:59Unlike the datasheet for BlueNRG-2 (https://www.st.com/resource/en/datasheet/bluenrg-2.pdf ), the BlueNRG-1 datasheet (https://www.st.com/resource/en/datasheet/bluenrg-1.pdf ) lacks chapter bookmarks. I really miss them because it's more difficult to navigate to particular spots in the 184 page document without bookmarks.Would some kind person @ST please consider replacing the sans bookmarked version of bluenrg-1.pdf with one that has the chapters bookmarked? Thank you in advance#bluenrg-1 #documentation-feedback #datasheet
Posted on June 27, 2018 at 14:46Hello,what is the best way to import a cube BLE project (for example C:\Program Files (x86)\STMicroelectronics\BlueNRG DK 2.0.2\Projects\Projects_Cube\SensorDemo_New) into AC6 System Workbench for STM32 ?I have generated from cubex an AC6 project for STM32L475RE. But now i want to incorporate into this project a blueNGR example.Thanks for any supportBest regards#bluenrg #ac6-system-workbench-for-stm32
Posted on June 21, 2018 at 07:53I am using SPSGRF-868 module on a medical device. I am trying to get the connection established between acquisition board(transmitter) with the Main display board (receiver). Both have this module configured in P2P mode.I used a code base from STM32CubeExpansion_SUBG1_V2.0.0 - I am using F4 controller @ both sides.Essentially same code base.HAL_Spirit1_Init();P2P_Init();Seems to do its job. Confirmed SPIs CLK and other things.P2P_Process @ receiver side does not receive anything. Perhaps, sending is not proper. Not sure.I am setting state machine to SM_STATE_START_RX for receiving and SM_STATE_SEND_DATA for transmitting before P2P_Process call.Only change in my implementation is GPIO IRQs (Tx/Rx) are not configured. In my board the module GPIOs(all 4)are grounded and NOT connected to processor. Is it necessary to connect and configure for this code base to work?Looking forward..Thank youGuna#spsgrf-868 #spirit
Posted on May 27, 2018 at 20:14 Hi, I'm using the BlueNRG-MS as HID peripheral and having trouble with the re-connection process. In order to reconnect with the central, I use directed advertising. The central recognize the slave and I get pairing complete event. The problem is that HID service remains encrypted for some reason and thus I cannot send HID reports (GATT services works). I can see that the device is connected. What is the correct procedure of initiating a reconnecting between bonded devices ? pseudo code will be welcome. Thanks, Yon Note: this post was migrated and contained many threaded conversations, some content may be missing.
Posted on June 29, 2016 at 12:27Hello All.I've been looking at using the ST7590 OFDM Power Line communications module in a project. However I've found the information published on STs website to be very lacking in technical details. From what information is available I'm sure that it can do what I need and do it well but I have no idea how to make it do it.I've raised a support ticket with ST asking for interface specifications, such as UART baud rates, timings, and pin functions, as well as what setup / initialisation procedures or required; and to be polite drawn a blank. The best that they could furnish me with was a C Header file overview from one of their dev boards, which was totally useless. As knowing what something does is totally different to my need of how it does it.Has anybody got any experience of using this device? and / or can anybody point me in the direction of the information I need to actually utilise the chip.Many thanksRussell
Posted on February 12, 2018 at 12:33Hi, I got my STEVAL-IDB007V1M with the SPBTLE-1' (based on BlueNRG-1 and installed the STSW-BLUENRG1-DK (v2.6.0). With the help of Antonio (https://community.st.com/0D50X00009XkWquSAF) I know, the STEVAL-IDB007V1M works as it should.I installed Atollic TrueSTUDIO for STM32 9.0.0, I imported the BLE_SensorDemo project as described in 'SensorDemo_BlueMS_main.c File Reference'. I can build the project - when I flash the Release.hex file to the BlueNRG-1 with the 'BlueNRG-1 Flasher' nothing happens on the BlueNRG-1.Same with Micro_Hello_World :(What's wrong?I set the HS_SPEED_XTAL=HS_SPEED_XTAL_32MHZ in BLE_SensorDemo and I already switched the optimization level to -O0 in the compiler settings of the projects.TIA, best regardsWolfgang
Posted on June 18, 2018 at 21:00Hi,I have been working with the blueNRG mesh network library, and have been looking into the demo lighting application using two IDB0008V2 boards. I have noticed that to provision the unprovisioned nodes to the network you have to use the android or ios application to do this. I was wondering is there was a way to make one of the development boards the provisioner. If this functionality is not available what solution would you propose?
Posted on June 17, 2018 at 03:24In my application, we are reading large files from an SD card and transferring them over WiFi to an AP. The SPWF04 is connected to an STM32L4 using UART.Data chunks are sent from the MCU to the WiFi module after opening a socket using the command AT+S.SOCKW and each time we wait for an AT-S.OK before sending the next data chunk. This works fine but after a while, the OK message doesn't come, resending data with AT+S.SOCKW doesn't help and the transmission gets stuck.This happens randomly and we are not sure how to debug.Thanks for your help!
Posted on June 15, 2018 at 17:21Hi,App note AN3975 references a zip file, is that still available?Thank you,Bruno#an3975-st7590
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.