Associate II
Jul 12, 2018 2:59 PM UTC
Question
PB for L152RE: UART1
- 1 reply
- 1256 views
Posted on July 12, 2018 at 16:59
Hello,
I have a pb with UART1 for L152RE board. I connected a sensor to my board in UART2 through a Max232 and i succeed to have information to my hyperterminal (TerraTerm). But i was not able to have information in the variable (or buffer) in my code. I was told that UART2 can not do that, so i was adviced to use UART1.
So i did it with UART1 but i'm not able to get data neither through hyperterminal nor in the variable in my code.
To parametrize the code, i use CubeMX and i changed the main.c. Do i have to change something else?
Find attached my code.
Thank you for your help.