Get ready for the STM32 Summit 2026 | Online, November 3
Raise questions or provide feedback on our community platform.
Most recent activity
Let user ability to remove their post.
This conversation lack the latest two posts that were present in the old community
Browsing the main forum at https://community.st.com/, possibly I hit Show More Activity and then a duplicate shows up:But there is no duplicate thread, it is just listed twice. Forum is forcing me to choose a product area for this, despite it being in the feedback forum. There is no relevant selection.Also no relevant tags that I can see.
Heyho,please move the code insertion tag out of the “...” dots menu to the “main menu”.And improve its visibility.This will hopefully make (new) people use it more.We all know how unreadable it is otherwise, and “hiding” the tag surely does not help.
@Lina_DABASINSKAITE The forum seems to no longer explicitly identify which users are ST Staff.I think it should.
I noticed knowledge base articles don’t have a date and the sorting order can’t be changed(‘most recent post’, ‘most recent comment’,...). Is that intentional, and are they sorted by ‘most recent post’?
When going through many pages of topics, clicking the Show more activity button, when you go back to the main thread from a topic, all the topics you’ve gone through are collapsed. So you have to click the Show more activity button a bunch of times all over to resume where you left off. Though you can right click and open a new tab, sometimes you may forget. Also, why was the page selection removed from the previous forum version and this one? I was hoping this new one would bring it back. :(
I posted on 3rd June and have received emails today saying i have replies. However the topic has now vanished! It is no longer on my topic list or reply list. When i click the link it goes to the main page!!Whats going on!? Hello RAdam.1, Your topic recently received a reply.Topic: STM32WB05 reboots when starting to advertiseDate: 2026-06-03 10:49 AMDid it solve your problem?Click here to view the reply and mark one as an Accepted Solution.This helps others find helpful answers in the community too!Thanks for being a STMicroelectronics Community member.Your STMicroelectronics Community TeamSTMicroelectronics Community sent this message to richardadamsla@gmail.com.Don't want to receive emails from us? Just click here.
Neither in the front page listing, nor in the individual forums. New threads used to be highlighted in bold on the old forum.
Example: Could be because it is a start post. But I find it useful to be able to quote specific parts of a start post and reply to those specific parts.
The following items were not carried overIt seems that Following & Followers were also not carried over ?(not that I’m concerned by this - just an observation)
Just for fun...i tried to use the SPI on H743 by direct setting and writing to registers:- i never got it working on some attempts years ago, so just used HAL , which just works.- now i tried again: cannot be, its so difficult...- ok, its a over complicated construction....old SPI on F303 works instantly and fast, no problem there.- but now have AI ... can it help?So i tried Sidekick, it should be easy for him...it...whatever...I asked how to do...in German, more easy for me - and a test: can it understand...?Sidekick tells:3. ZusammenfassungUm auf dem STM32H743 einen SPI-Transfer durch Schreiben auf SPI_TXDR zu starten, müssen Sie:Die Datenlänge im SPI_CFG1-Register korrekt einstellen,die Bitreihenfolge im SPI_CFG2-Register wählen,die relevanten GPIOs konfigurieren,das SPI-Modul aktivieren,und dann die Daten in der konfigurierten Länge auf SPI_TXDR schreiben.Ein Schreibzugriff mit weniger als der konfigurierten Datenlänge ist nicht zulässig.--- THIS didnt help me, as it also just brin
Wasn't anywhere near ST site but got this email:Please click on this button to start the download of the requested content:${ctatext}Was this a test gone wrong? Did anyone else get it? Do I need to contact support?Just posting here in case anyone else got it.
Hello,would like to change the email address on my ST Community account. I cannot find the option in the settings. Could an admin assist with updating my email? Thank you!
2026年,1月30日,STM32 Sidekick看不到了。出故障了吗? Google translation: On January 30, 2026, the STM32 Sidekick was no longer visible. Was it malfunctioning? Please note that the language of the forum is English - see the Terms & Conditions.
I get this error when I press the 'Kudos' button: https://community.st.com/t5/stm32-mcus-products/stm32g411-availability/m-p/885372/highlight/true#M293512 Also happens on other posts in that thread, and in other threads. Looks like a recurrence of Kudos button gives error (12 Dec 2025)
Had a few of these these morning
I've seen it a couple of times - both from ST Employees, IIRC; eg,https://community.st.com/t5/mems-sensors/lsm6dso-and-lsm6dso32-compatible/m-p/891941/highlight/true#M27029 Neither the button nor the option allows just formatting a single word like that. Looking at the HTML view of the above post, it's using the <code> tag - but I don't see any way to enter that via the Editor?(I did that one via the HTML editor - but that's very klunky!)
Tried to paste code in reply. Noticed, that line count does not match. Clicked in editor and it started to duplicate.Also check out attached video.In order to reproduce the bug, longer code must be pasted in C code insert tool from tool bar. Then mouse pointer must be navigated at the end of inserted code and clicked few times here and there. Inserted code will start to duplicate in editor.
For the past week or so, pasting images directly into posts seems to have broken.I used to be able to just take a screenshot, or copy an image and paste it straight into the editor, but that no longer works.I press 'paste', and nothing happens - no error messages or anything.I am now having to save the image locally, and then use the 'Insert Photos' button to import it. There is history with this, but now it seems to have just broken completely. Using Chrome Version 145.0.7632.109 (Official Build) (64-bit) on Windows-11 Pro
Between Last Day to Last Year, doesn't show users. Only All Time shows users.
144 characters
Or 'Feature Request' or similar.Applies to CubeIDE, CubeMX, and CubeMX2 - probably also others ...eg, see here and here.
My post was deleted without any notification or reason? https://community.st.com/t5/escalated-topic/stm32h5-fdcan-system-bootloader/m-p/886189#M30060
so it seems:https://community.st.com/t5/stm32-mcus-embedded-software/sd-card-no-file-system-error/m-p/641421/highlight/true#M45513On other forums, the 'Mark As Solution' just changes to 'Unmark Solution' (or whatever) - so it's always obvious, and in the same place. Addendum:Perhaps this: https://community.st.com/t5/stm32-mcus-embedded-software/sd-card-no-file-system-error/m-p/641422/highlight/true#M45514 could be added here: https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.