Get ready for the STM32 Summit 2026 | Online, November 3
Raise questions or provide feedback on our community platform.
Most recent activity
When editing a post, the strikethru (like this) style is missing. I clicked the area where the "..." should be to be sure there is no button. This is definitely a new bug. I could edit posts with strikethru before. Have noticed it a few times lately. Tried reloading the page. Nothing. Came back 15 minutes later and it shows up again. Re-looking at this screenshot of the issue that I took, maybe I should have clicked the "back" icon on the left? I don't know what that would do. It's there when creating a post: But it only happens sometimes. On other posts, it's clearly visible:
Example image without zoom controllRe: ThreadX thread and queue names not displayed p... - STMicroelectronics Communityexample with zoom controll i cant found now , but sometimes is showed bottom on image and i mean this zoom control is required on all any image.
hi would like to request REACH 240 report. Please assist thanks.
Doesn't happen in the thread itself: https://community.st.com/t5/stm32-mcus-embedded-software/stm32l4-hal-rtc-functions-do-not-check-hrtc-gt-instance-before/m-p/703427
These two notifications refer to the exact same post:He couldn't have mentioned me without making a reply, so I really don't need two separate notifications!EDITAnd why are the two email notifications sent 7 minutes apart?!
This notification is incorrect. This user created a new topic and did not reply in this topic: This notification is also incorrect:Two unrelated notifications got merged. I saw this happen once before and I was confused about it.I use Firefox.
Please forward vote against forced forum password resets due to expiration. It’s very old school security model.
1. It's useless.As it's not curated, the vast majority of links is entirely irrelevant to given post. Machines are too ***, even if you call it AI.2. It's harmful.It provides false keywords for external search machines such as google, making it harder to find genuine content.3. given 1, and 2, it's just pure waste of bandwidth.JW
Please forward this message to the MCU development team.The ST Microelectronics MCUs still use old school techniques and supports the coin-type polyacene capacitor battery and external crystal oscillators, despite advancements in semiconductor designs. Practically, extremal crystal oscillators are no more used and on-chip high performance and relatively cheap oscillators have replaced such an approach! Additionally, super capacitor backup power is no more used in advanced designs and memory cells can still retain the charge using more advanced techniques!I am not here to explain all such advanced circuit design techniques but would like to point out the out dated conventional methods still used by ST Microelectronics!
I kept coming back to this website to download the STM32 Cube IDE and the servers would always be down once I tried to log in and download it.I've noticed some forums from 2019 mentioning similar problems with how slow the website is responding, so it's great to see that this website is still suffering from network maintenance and bad optimization...Seriously, what is wrong with this website ?? literally had to wait a few days to download the IDE, and now I'm trying to download the STM32CubeMX and this website still pends forever... I can click on buttons and functionalities, but this slow website is always unresponsive when it comes to downloading stuff
I've just clicked at this link (which came to be thanks to several botched migrations) in this thread, to get this message:I am not paid by ST to handle user interfaces, thus have no intention to write a mail to that address, explaining, that this is to be handled in a more, let's say, intelligent way. @Lina_DABASINSKAITE , can you please do that for me.Thanks,JW
What should I do if nobody is answering my question?
Subj.
The "whole question in the title" problem seems to have largely gone away, but now we get the opposite - unhelpfully short titles!Only today:So perhaps the 'Posting Tips' need an update ?https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228@Lina_DABASINSKAITE
Searching for "module" includes hits for "modulation" :face_with_rolling_eyes: :frowning_face: :thumbs_down: Sure, it can be useful to have "fuzzy" searches like this when you're not quite sure of the term you need - but there really needs to be a way to limit searches to just the exact term entered.Basic search options:Any combination of 1 or more of the words enteredAny combination of all of the words enteredOnly the exact phrase entered
If A asks a question and B replies. If B subsequently returns to edit her reply the prompt she gets above the edit box is "Edit your reply to B". Which is wrong, it should be "Edit your reply to A". More simply, why not just have it say "Edit your reply" and be done with it?
See for example this helpful post by @Andrew Neilhttps://community.st.com/t5/stm32-mcus-products/stm32-ic-s-unique-id/m-p/657372/highlight/true#M239912 Andrew is a stand-up guy. He wouldn't be this sloppy when posting, but it's not his fault.Whenever someone inserts a "Code" block, in order to get syntax highlighting. Any subsequent edit of the post adds an extra blank line above and below the block. It doesn't matter if you erase them when you edit. They can only grow,like the mythical hydra. The only solution is to remove the code nlock entirely, delete all the blank lines and save the post. Then edit it again, and re-insert the code-block. Then, you must never-ever-ever edit that post again, or you'll have to go through it all over. Come on ST. 2024. AI. 32TOPS in every phone within 5 years. Can we fix the editor please???
Just remove it. We don't need it. We have the feedback forum. JW
When you subscribe to a thread with multiple participants and a single participant adds a reply, you get a notification.But the title of the notification includes the name of everyone in the thread who have commented so far ("A and B replied to topic", "X and 2 others have replied", etc') rather than the most recent post which triggered the notification. If there have been multiple comments since you last visited the thread, it's fine to "roll-up" all the comments into a single notification, but if there's only been one comment it's less useful. You might as well just write "a new comment was added to the thread", without naming anyone. This behavior doesn't occur in "Recent notifications" - it just tells you who posted like it should. This looks like a (small) bug to me.
eg, does the v1.15.0 thread still need to be 'pinned' now that v1.15.1 is there?:thinking_face:
..
Sometimes (often :frowning_face: ), the OP disappears without marking a solution - even when it is obvious that a solution was found.In this case, I sometimes see that ST Staff will mark the solution.This seems fine to me, but I think it would be good to distinguish when this has happened.eg, here:https://community.st.com/t5/stm32-mcus-products/what-is-the-smallest-achievable-delay-in-microseconds-for-a-16/m-p/684830#M251961The notification tells me this was marked by ST (@mƎALLEm ) - not the OP:But there's nothing to show that in the thread itself.On the TI forums, they do separately identify, "TI marked this as the solution"
After some period of approximately 2 years my login is rejected as having incorrect username or password. Careful reentry is not successful, I keep getting the same rejection. I conclude that passwords expire after some time.If that is true, why not a message " Your password has expired. Please create a new password" to avoid fruitless attempts to reenter the password that worked the day before?Or correct me if I have the wrong assessment of the problem.
For example here:https://community.st.com/t5/stm32-mcus-products/timer-compare-output-using-dma-stm32f3discovery/td-p/672897there are two code blocks with "View more",buttons. When "View more" on the first code block is clicked, both code blocks are expaneded. However, the "View more" at the second code block remains, and if clicked, nothing happens just that "View more" button disappears.I don't think this is the expected behaviour.JW
The ST community site is often extremely slow, even time outs occur . You access a few pages fine and then it takes a minute or more , time out or error occur.Often trying to Edit a port, it often fails with an error message. Accessing other website is no problem at all.
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.