Skip to main content
BarryWhit
Lead
Jul 1, 2024 8:36 PM UTC
Solved

The post editor loves blank lines so much, it puts them on everything

See for example this helpful post by @Andrew Neil

https://community.st.com/t5/stm32-mcus-products/stm32-ic-s-unique-id/m-p/657372/highlight/true#M239912

 

Andrew is a stand-up guy. He wouldn't be this sloppy when posting, but it's not his fault.

Whenever someone inserts a "Code" block, in order to get syntax highlighting. Any subsequent edit of the post adds an extra blank line above and below the block. It doesn't matter if you erase them when you edit. They can only grow,

like the mythical hydra. The only solution is to remove the code nlock entirely, delete all the blank lines and save the post. Then edit it again, and re-insert the code-block. Then, you must never-ever-ever edit that post again, or you'll have to go through it all over.

 

Come on ST. 2024. AI. 32TOPS in every phone within 5 years. Can we fix the editor please???

 

 

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
Jul 1, 2024 8:52 PM UTC

Indeed - Already reported by @waclawek.jan:

https://community.st.com/t5/feedback-forum/don-t-litter-posts-with-whitespace-empty-paragraphs-inserted/td-p/574693

 

EDIT:

There's a workaround to somewhat mitigate it:

https://community.st.com/t5/feedback-forum/don-t-litter-posts-with-whitespace-empty-paragraphs-inserted/m-p/668939/highlight/true#M1347

but the forum keeps adding them back in.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

2 replies

BarryWhit
BarryWhitAuthor
Lead
Jul 1, 2024 8:37 PM UTC

Like this

 

 

 

 

 

 

 

Give me some space!

 

 

 

 

 

 

 

... See?

"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
Andrew Neil
Andrew NeilBest answer
Super User
Jul 1, 2024 8:52 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.