Skip to main content
waclawek.jan
Super User
Jul 19, 2023 6:00 AM UTC
Question

Yellow "Feedback" is annoying, takes time to load and occupies space

Just remove it. We don't need it. We have the feedback forum.

JW

This topic has been closed for replies.

12 replies

Lina_DABASINSKAITE
ST Community Manager
Jul 20, 2023 8:10 AM UTC

Hello @waclawek.jan , 

Thanks for letting me know. Could you elaborate more how long it takes to load and if possible, screen-record it? Also, please include your browser. Having this, I could investigate the issue. On my end it seamless and very fast. 

For now, there are now plans to "Remove" the extension because it's part of ST's broader ecosystem to gather feedback. I am sorry that you find it annoying. 

BR,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
waclawek.jan
Super User
Jul 20, 2023 12:37 PM UTC

It's on mobile phone, I am not able to measure that, but whatever it takes it's more than zero which is exactly how much is needed.

Because we don't need this feature. So, just remove it. Feedback gathered in this way is useless, and it's annoying. Do you want users come here? Then stop annoying them, they are not interested in providing you THIS kind of feedback, there is the feedback forum for this purpose. Users are not interested in broader ST ecosystems.

Besides, on the mobile, it also obscures the up-arrow, which we (technical users who know how to navigate a browser natively) don't need either... (lazy to link the thread where I posted that).

Is the "user first" principle something ST does not subscribe to?

JW

 

 

waclawek.jan
Super User
Jul 21, 2023 1:10 PM UTC

Observing page load on a PC (and yes, loading 1400 icons even from cache takes seconds, especially on a system with rotary disc, and is annoying: ditch icons, use Unicode icons if you must) I've realized that together with medalia you've added half a dozen other spying services, presumably as part of the "broader ecosystem". That might also explain the longer loading times on mobile, especially on a not-that-perfect network.

Please remove them from the forum. Letting 3rd parties spy on your users is not a decent thing to do.

JW

Lina_DABASINSKAITE
ST Community Manager
Jul 25, 2023 5:28 PM UTC

Hello @waclawek.jan , 

Regarding the Medalia, I take it to investigate if there any possible improvements for the mobile version.

The Page load issue: could you please be more specific on how long exactly it takes, mobile browsers you use, and your mobile OS? We did not notice any page load performance issues, so I would we be happy to have a further look into it. 

As for "spy services", I can assure you there are no such things. We use standard web traffic analytics tools and Medalia as Feedback extension across all ST. So really nothing to worry here about :). 

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
waclawek.jan
Super User
Jul 26, 2023 1:21 PM UTC

> standard web traffic analytics tools

Yes. You may call using 3rd parties (and not one, but a bunch of them) to gather data on users "traffic analytics tools"; but at the end of the day, it's just spying and a despicable thing to do. That others do it too is no excuse.

JW

Tesla DeLorean
Guru
Aug 19, 2023 5:35 PM UTC

Annoying me today, large yellow bar in the way of edit / post window. Either accidentally hitting it or randomly popping up. Using from phone today.

Do not like, do not want

Stop using the wrong metrics to drive decisions. You draw the wrong conclusions, and make poor decisions.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
STOne-32
ST Technical Moderator
Aug 19, 2023 7:11 PM UTC

IMG_4566.jpeg

IMG_4565.jpeg

IMG_4564.png

IMG_4563.jpeg

Dear @Tesla DeLorean  @waclawek.jan ,

Thank you for the feedback, I’m wondering if there is a recent change observed these days ? And why is this annoying…  is it the frequency of « feedback » button to appear in random way etc. As explained by @Lina_DABASINSKAITE , we are focusing on our community experience and we need both qualitative and quantitative real-time feedback and satisfaction to react accordingly, we can not rely on long period feedbacks . Here is my experience just writing this reply : 4 screenshots on a 6 inch display.

Thanks again for your valuable feedbacks !

STOne-32

Tesla DeLorean
Guru
Aug 19, 2023 10:47 PM UTC

It's annoying because I don't want things popping up whilst typing.

Accidently touching the side of the screen seems trigger one type of pop-up. There you can't exit when you selected stars unless you add a reason.

The yellow bar appears and often covers part of the Reply Button or arrow.

The other popup seems random, perhaps time based, that one allows stars to be selected and submitted without giving a typed in reason.

In post edit the yellow obscures the Post button, but most annoying is that it keeps moving or aligning with the screen. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RhSilicon
Lead
Aug 20, 2023 6:42 AM UTC

If that yellow tab can be annoying, imagine half the screen being blocked like this:

ST_WEBSITE_DOH.png

 

Homer-DOh

waclawek.jan
Super User
Aug 20, 2023 6:42 AM UTC

You are receiving honest, detailed and well-though feedback from users who are invested in ST and this Forum, and who have track of contributing, here.

And then you have a potentially high amount of anonymously gathered one-to-five-stars information, with absolutely no relevance to any particular issue, submitted under annoying situation (unwanted popup) with clear potential for bias, from users which are mostly one-time visitors with little to no incentive to help the site, mediated by a shady company specialized to gather data over which you have no control.

The former is known to be ignored by you, or even having annoyed some of you.

And now you are saying the latter is somehow vital for you.

JW

TDK
Sep 12, 2023 4:06 PM UTC

Just dropping a note here to say these constant feedback requests are still annoying. There is no need to bug me weekly to get my feedback. My feedback is that you should stop annoying me with feedback requests. My feedback the next time you ask me will be that you should still stop annoying me with feedback requests.

The feedback requests on the general st.com site that function as a popup and prevent you from interacting with the site are awful. It feels like an ad on a shady website that tries to get you to click the ad, except that somehow ST is complicit in it.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
Jun 27, 2024 9:40 PM UTC

It jumped at me again.

This time it did not allow me to add a comment. So, I write here, what I wrote there all the zillion times it jumped at me in the last months: "ditch medallia". So you don't need to guess who was that. I was.

It is still annoying. Just remove it, no discussion.

JW