Skip to main content
This topic has been closed for replies.

5 replies

Lina_DABASINSKAITE
ST Community Manager
Jun 7, 2024 9:45 AM UTC

Hello @MM..1 , 

Thanks for sharing your request. I will see what we can do about it and get back. 

In the meantime, I suggest using a workaround following these steps: 
1. Right mouse click on the image
2. Select "Magnify image" 

This will allow you to have a zoom in / zoom out option. 

Cheers,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
Jun 7, 2024 1:17 PM UTC

Definitely see inconsistency, perhaps related to the image type. ie for PNG but not JPG ?

Also find the two-point finger stretching on Android is frustrating, and also having to down load attached images to see them.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Jul 23, 2024 4:33 PM UTC

Hi @MM..1 @Tesla DeLorean ,

Could you please share a direct link when you come across an image with the zoom control you are referring to? We need an example to be able to investigate it.

Best,

Adam

MM..1
MM..1Author
Super User
Jul 23, 2024 5:04 PM UTC

Error in final launch sequence - STMicroelectronics Community attached png show zoom

normal images no. But on my notebook with 2560x1440 14inch is ...

Aug 13, 2024 8:24 AM UTC

Hi @MM..1 ,

Zoom controller is currently only available for file attachment previews. We will pass along the topic to the developer team to understand the effort involved in adding a zoom controller for images in posts. Depending on the estimation, we will decide how to move forward with this topic. We will keep you posted.

Best,

Adam