Read our guidelines, share your thoughts about your community experience, and explore community insights.
Most recent activity
Hi,When I posted a question, the following warning message appeared on the post:Marked as spam.This is the URL for my post.https://community.st.com/t5/stm32-mpus-embedded-software-and/sd-card-read-issue/m-p/881342#M5615This post doesn't appear on the forum board and can't be found through searches...Best Regards,Karsten
See: STM32CubeMX 6.17.0 released by @Aimen1 The link to Getting started with Programmable Logic ArraY (PLAY) - stm32mcu is wrong:Link is: https://wiki.st.com/stm32mcu/wiki/Getting_started_with_Programmable_Logic_ArraYshould be: https://wiki.st.com/stm32mcu/wiki/Getting_started_with_Programmable_Logic_ArrayBut even with the correct link, the page is empty: And why is the URL case-sensitive anyhow? PS:In fact, there seems to be no information at all about this anywhere - see: So what's all this "PLAY (Programmable Logic Array) on STM32H5 4M" stuff, then ?
eg, here: It often seems to be used by "accident" by beginners.In this case possibly because, in the "extended" toolbar, it's in the place where 'insert image' was on the "basic" toolbar:
Hi,Using Safari 26.2 I'm unable to delete or edit my own posts. Does anyone else
The conversation window with the company's chatbot exhibits a glitch.Specific manifestation: The window flickers when inactive.Trigger method: After posing a question and receiving the AI's response, scroll down to the bottom of the conversation window using the mouse wheel immediately after the reply concludes to reproduce the bug. (This has only occurred once thus far; subsequent testing failed to replicate the issue.)The ST Community moderator has edited the post to comply with the ST Community language: English. For more information, see: ST Community Terms and Conditions.Translated with DeepL.com (free version)
See:https://community.st.com/t5/stm32-mcus-boards-and-hardware/struggling-with-a-simple-uart-printf-on-nucleo-g474re-works-on/m-p/874056/highlight/true#M29428 Sidekick says UART2, but the User Manual & Schematics show LPUART1 (default) or UART1 (by changing solder bridges):UM screenshot: https://community.st.com/t5/stm32-mcus-boards-and-hardware/struggling-with-a-simple-uart-printf-on-nucleo-g474re-works-on/m-p/874047/highlight/true#M29425Schematic screenshots - by @mƎALLEm:https://community.st.com/t5/stm32-mcus-boards-and-hardware/struggling-with-a-simple-uart-printf-on-nucleo-g474re-works-on/m-p/874051/highlight/true#M29427
It's been sat there "thinking" for several minutes now!Just putting "NUCLEO-G474RE VCP" did get an answer
Hello, I can't download any software from this, I mean st.com. After popup with License Agreement download doesn't start. I am only one with this issue? Problem occurs on Mozilla Firefox. On Chrome it works fine.
The new STM32CubeIDE 2.0.0 workflow tutorial covers only C - not C++ See: Create a new stm32 project correctly on 2.0.0 and use C++ for it. Edited to correct 2nd link.
Tody I got an email notification: "The post Re: Is STM8 recomended for beginners? was moved by Maxime_MARCHETTO1. Reason: Post removed due to generative AI. Explanation: Breach of the ST Community guidelines for AI content use case: https://community.st.com/t5/community-guidelines/why-predominantly-ai-generated-posts-and-replies-on-the-st/ta-p/633785"I have never used AI to generate any text for a forum post, neither on this nor on any other forum. I cannot see which post was removed, since the link to the removed post just gives me an "Access Denied" error page.The linked Community Guidelines only state that AI-generated posts will be removed, and "in some cases" the users banned. However, I see no information on how ST determines if a post is AI-generated, how users can appeal decisions, how false positives of whatever mechanism ST uses will be handled.
In this post, clicking on preview of the relatively large txt attachment, scrolling down to its end reveals a "Download file" button. Clicking on that button displays a surprising "this file could not be downloaded" message. The file can be downloaded normally, though.JW
Here:https://community.st.com/t5/stm32-mcus-products/stm32f7-hard-and-memory-faults/m-p/866383/highlight/true#M290480The red message appears on clicking the 'thumbs-up' button. Win-11 with Chrome browser: Version 143.0.7499.42 (Official Build) (64-bit) PS:Chrome just updated itself to Version 143.0.7499.170 (Official Build) (64-bit) - no change.
The "Virus scan in progress..." message is gone, but attachments are still behaving funny. Issue 1: 2 out of the 3 attachments here cannot be accessed. Clicking on them does nothing and the "download" icon is missing. https://community.st.com/t5/others-stm32-mcus-related/facing-difficulties-in-interfacing-stm32l433-mcu-to-vcnl4040-i2c/m-p/861339 Issue 2: I've also noticed that image attachments can't be viewed directly in the past week or so. Trying to click on the png attached here shows an error instead of showing the image. https://community.st.com/t5/stm32-mcus-products/stm32l433rct-freezing-lock-up-problem/m-p/865559/highlight/true#M290358 The download icon works and once downloaded the images can be viewed directly. They appear to be valid PNG files. Seems forum functionality is going backwards. Split this to a new thread if you want. Seems related IMO.
Post moved from STM32 Sidekick announcement It doesn't seem to work with Firefox (146.0), the yellow icon appears and immediately disappears, Regards,Hans.
Here - since at least 10:56 GMT:https://community.st.com/t5/stm32-mcus-boards-and-hardware/nucelo-stm32h563zit6-internal-temperature-sensor-issue/m-p/861430 and here - since at least 08:38 GMT:https://community.st.com/t5/others-stm32-mcus-related/facing-difficulties-in-interfacing-stm32l433-mcu-to-vcnl4040-i2c/m-p/861339 That's just the 2 I've seen ...
See: https://community.st.com/t5/other-hardware/equation-error-lmx35-lm135-lm235-lm335-temperature-sensor/m-p/722841/highlight/true#M28592The post editor allows me to create multi-level subscripts, and it displays fine in the editor:But, when I post, I get the "Invalid HTML" error, and the post loses all the subscripting:Is this intended behaviour?To be able to subscript would be useful. PS:So the HTML is not invalid; it may be unsupported - but it's not invalid.
Here, in the thread "Over Current on STM32 Board", the same thread is listed as 'Related Content' !:face_with_tears_of_joy:It's not "Related" content - it's exactly the same content! I think this happened because I came to a specific post within that thread (from a Notification) - rather than a link to the top of the thread?
Hello ST Team, I registered for the upcoming STM32 Summit | Workshops in Bengaluru (December 5, 2025) more than 8 days ago using my email address, but I have not yet received the official invitation or confirmation mail. Since the event date is approaching quickly, I wanted to check if there is any additional step I need to complete, or if my registration is still under review. Could you please confirm my status or guide me on how to proceed? Details: Name: Abhilash Maddineni Registration date: Nov 21, 2025 Thank you for your support. I am eager to participate in the Summit and don’t want to miss out due to a pending invitation. Best regards
Hello there I would like to share my source code with @mƎALLEm. for troubleshooting purposes. How can I get permission to share my files via .zip in private messages?Thank You! Julian
Split from Valid login details ignored as this is unrelated.Great thanks ST.
On a related note, and because of recent observation, I have a question. Does the ST forum / community site scan user-uploaded files a.k.a. attachments for malware / trojans / viruses ? Since this forum makes it easy to embed graphics (like screenshots) directly into a post, I never download and open any attachment that is not text format. Posts with e.g. alleged screenshots attached as image file look suspicious to me.--- This content was split from this discussion Data leak from st.com ?ST Community team
It has CubeIDE and CubeMX - but not CubeProgrammer. Should there also be "ST-Link" and/or "Debugger" ? Example where these would apply:https://community.st.com/t5/stm32-mcus-wireless/how-to-solve-quot-error-no-stm32-target-found-quot-using-nucleo/td-p/856618
Hello ST Community team I would like to report a possible issue with the contributor ranking in the “Best Answers” leaderboard. For example, when applying the Last 24 hours filter, I noticed that two contributors appear ranked as #20 and #21 on the first page: But on the second page, the same contributors are shown as #24 and #25: The screenshots were taken at 10:20 GMT. Could you please check and correct this inconsistency in the ranking display? Best Regards. II
This has happened before, but I can't seem to find the thread.At the forum login, I enter correct details.The forum thinks for a while, then just re-presents the blank login form - no messages about invalid details.Happened just now, and once last week.Chrome browser on Win11-Pro
Hello - I posted the question online and brought up concerns that the example code does not work. To this day, it still does not work, however the staff marked it solution when we haven't solved the issue. I don't think that's appropriate, it is hard enough to try to get attention to my post.
ST Community highlights – April to June 2026
Already have an account? Login
No account yet? Create an account
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.