cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 Camera with STM32F7 Discovery board?

Xav Cachan
Associate II
Posted on February 19, 2017 at 20:59

Hi all,

I'm trying to use the camera

STM32F4DIS-CAM

with my STM32F7 Discovery board, with Keil uVision IDE. I have downloaded STM32Cube, and in the examples there is a BSP directory, with BSP drivers examples, including a camera.c for the camera. All the drivers are working well (LCD, Touchscreen, audio, sram...), but the programm stops when the Camera example starts. It seems that the initialization is OK, I can see 'QQVGA camera stream', but then nothing happens, the stream is only a white screen, and the touch actions do not work (change brighness, contrast...). The 'user button' also do not work anymore...

Do you have an idea of the way I should follow to solve such problem?

Thank you.

Best regards,

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on March 01, 2017 at 19:11

Hi all,

I have finally found a solution: it seems that the stm32f7xx_it.c (version 1.1.0) in the BSP camera example of STMCube for STM32F7 is badly written. As a conclusion, the programm goes into infinite loop and the screen is white.

For my solution, all the changes have to be done in stm32f7xx_it.c file (maybe ST should modify the file included in the STMCube_FW_F7 package):

1. at the beginning of the file, include the camera handler with

/* Camera handler declared in 'stm32746g_discovery_camera.c' file */

extern DCMI_HandleTypeDef  hDcmiHandler; 

2. Modify the function DMA2_Stream1_IRQHandler as follows:

void DMA2_Stream1_IRQHandler(void)

{

  //BSP_CAMERA_DMA_IRQHandler();

    HAL_DMA_IRQHandler(hDcmiHandler.DMA_Handle);

}

3. Modify the function DCMI_IRQHandler as follows:

void DCMI_IRQHandler(void)

{

  //BSP_CAMERA_IRQHandler();

    HAL_DCMI_IRQHandler(&hDcmiHandler);

}

Everything works fine now for me. Hope it will help.

(Thanks to Aditya Manglik web site, it gives some interesting hints!)

Best regards,

Xavier

View solution in original post

6 REPLIES 6
Imen.D
ST Employee
Posted on February 22, 2017 at 19:42

Hi

cachan.xav

‌,

Maybe you should check and look more carefully atyour configuration. Then,I suggest you to debug, localize where the code hangs/stop,and the kind of message gives.

This will help toidentify what is the problem that you have.

Otherwise, you can share your code and debugger screenshot,thatwillbe easier for user forum to understand the issue andhelp you.

PleaseKeep me informed about your progresson this problem.

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on February 22, 2017 at 21:09

Thank you Imen for your answer ! I am so happy that someone tries to help !

For my project, I have only downloaded STM32Cube package, and opened the

uVision STM example proposed in the BSP directory. Then I have just

validated the camera.c in the main file, connected the camera to the

board, and tried to execute the code. Nothing else has been changed in

the configuration, so I do not understand what can be wrong.

I have tried to debug, please see the attached file. It seems that the

programm calls DMA2_Stream1 IRQ, but the corresponding ASM code shows

that we then stay in an infinite loop (instruction in 0x08001dD4C is

branch on ... 0x08001D4C).

If you have any idea...

Thank you again.

Best regards,

Xavier

Le 22/02/2017 à 19:45, IMEN D a écrit :

>

STMicroelectronics Community

<https://community.st.com/?et=watches.email.thread>

>

Re: STM32F4 Camera with STM32F7 Discovery board?

reply from IMEN D

<https://community.st.com/people/DAHMEN.IMEN?et=watches.email.thread>

in /STM32 MCUs Forum/ - View the full discussion

<https://community.st.com/message/147463-re-stm32f4-camera-with-stm32f7-discovery-board?commentID=147463&et=watches.email.thread#comment-147463>

>

________________

Attachments :

Camera_infinite_loop.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hytf&d=%2Fa%2F0X0000000bDd%2FBecdyj_DeujI8ltyj4OZQ3PulFA3i6GABagZeNfMHB4&asPdf=false
Martin.Sergio
Associate III
Posted on February 27, 2017 at 10:49

Hi

Cachan.Xav

,

Any progress with this issue...????

I have a similar problem with my STM32479I-Eval and the Camera Examples provided in STM32Cube_FW_F4_V1.0

https://community.st.com/0D50X00009XkasmSAB

Best Regards,

Sergio

Posted on February 27, 2017 at 18:40

 ,

 ,

Hi Sergio,

No, I am still trying to find why it does not work...

:(

Best regards,

Xavier

Le 27/02/2017 à 10:50, martin.sergio a écrit :

>,

STMicroelectronics Community

<,https://community.st.com/?et=notification.mention>,

>,

You have been mentioned

by martin.sergio

<,

/in Re: STM32F4 Camera with STM32F7 Discovery board? in

STMicroelectronics Community/ - View martin.sergio's reference to you

<,https://community.st.com/0D70X000006SRhfSAG

>,

Posted on March 01, 2017 at 19:11

Hi all,

I have finally found a solution: it seems that the stm32f7xx_it.c (version 1.1.0) in the BSP camera example of STMCube for STM32F7 is badly written. As a conclusion, the programm goes into infinite loop and the screen is white.

For my solution, all the changes have to be done in stm32f7xx_it.c file (maybe ST should modify the file included in the STMCube_FW_F7 package):

1. at the beginning of the file, include the camera handler with

/* Camera handler declared in 'stm32746g_discovery_camera.c' file */

extern DCMI_HandleTypeDef  hDcmiHandler; 

2. Modify the function DMA2_Stream1_IRQHandler as follows:

void DMA2_Stream1_IRQHandler(void)

{

  //BSP_CAMERA_DMA_IRQHandler();

    HAL_DMA_IRQHandler(hDcmiHandler.DMA_Handle);

}

3. Modify the function DCMI_IRQHandler as follows:

void DCMI_IRQHandler(void)

{

  //BSP_CAMERA_IRQHandler();

    HAL_DCMI_IRQHandler(&hDcmiHandler);

}

Everything works fine now for me. Hope it will help.

(Thanks to Aditya Manglik web site, it gives some interesting hints!)

Best regards,

Xavier

Posted on April 21, 2017 at 20:52

Cachan.Xav

,

Thank you so much for your fix to ST’s buggy BSP camera code.

I quickly diagnosed the problem since the two IRQs in question recursively call themselves until they runs out of memory.

However the solution was not obvious to me until I found your post.

It is a shame that such a reputable company as ST publishes buggy and untested sample code that wastes other people’s time and money!