2017-08-30 10:09 AM
I am trying to test the magnetometer on LSM9DS1 sensors.
Can I apply the same self-test range-values than the LIS3MDL compass to check the LSM9DS1? The fact is that the magnetometer in the LSM9DS1 seems to be a LIS3MDL (same documentation of the registers). I am using the
http://www.st.com/resource/en/application_note/dm00136626.pdf
, where the self-test procedure is explained in page 19, with self-test ranges indicated in table 17.I already implemented a self-test procedure for the LSM9DS1 and I obtained for one sensor on which I suspect a problem the following values:
Average_X_self_test - Average_X_no_self_test = 2551 (no scale) = 0,93 gauss
Average_Y_self_test - Average_Y_no_self_test = 2682 (no scale) = 0,98 gauss
Average_Z_self_test - Average_Z_no_self_test = -415 (no scale) = -0,15 gauss
And for a second sensor that seems ok, the values are:
Average_X_self_test - Average_X_no_self_test = -4476 (no scale) = -1,64 gauss
Average_Y_self_test - Average_Y_no_self_test = -4473 (no scale) = -1,64 gauss
Average_Z_self_test - Average_Z_no_self_test = -515 (no scale) = -0,19 gauss
Values are consistent on several runs of self-tests. And if I take the ranges mentioned in the application note of the LIS3MDL, it means that the first sensor is broken.
Thank you for your support.
Best,
David
#lsm9ds1 #lis3mdl #magnetometer #self-testSolved! Go to Solution.
2017-09-05 2:56 AM
Hello David,
as mentioned in another thread you can use
for LSM9DS1 magnetometer selftest including the limits. If the first sensor you mentioned is not broken than it's at least marginal.Regards,
Petr
2017-09-05 2:56 AM
Hello David,
as mentioned in another thread you can use
for LSM9DS1 magnetometer selftest including the limits. If the first sensor you mentioned is not broken than it's at least marginal.Regards,
Petr
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.