cancel
Showing results for 
Search instead for 
Did you mean: 

Why STM8 Discovery stops if Interrupts are enabled e.g. TIM4_IER is set and rim() is used?

BEner.1
Associate

//STM8 Discovery freezes if TIM4_IER is set or rim() is used

//please help, I'm using free mode Cosmic Compiler on STVD

#include "iostm8s105.h"

void init_port(void){

PD_ODR = 0x00;   

PD_DDR = 0xff; //output  

PD_CR1 = 0xff; //pushpull    

}

@interrupt test(void) {

TIM4_SR &= 0xfe; // Status register 

 }

void ini_timer4(void){

TIM4_IER |= 0x01; // Interrupt Enable reg 

TIM4_PSCR = 0x15; // Prescaler register 

TIM4_ARR = 0xf0; // Auto-reload reg  

TIM4_SR = 0x00; // Status register 

TIM4_CNTR = 0xaa; // Counter reg High 

TIM4_CR1 |= 0x01; // Control register  

}

void delaytime(void){

for(del=0;del<50000;del++);

}

void main(void){

ini_port();

ini_timer4();

rim(); //enable interrupt

while (1){

PD_ODR |= 0x01; 

delaytime();

PD_ODR &= 0xfe; 

delaytime();

}}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
BEner.1
Associate

Solved the problem already, it was caused by incorrect interrupt vector address.