cancel
Showing results for 
Search instead for 
Did you mean: 

urgent (read 3 ADC channel)

seesy123
Associate
Posted on August 22, 2013 at 13:17

first thanks for spenting your time to me. I need read 3 channel for AIN0,AIN2 and AIN3. But i cant get the analog reading. it always show me constant value even my analog input changed. I'll post related about ADC part..Please help me. thanks in advance

 // Initialisation of ADC

  

  ADC1_ConversionConfig(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_3, ADC1_ALIGN_LEFT);

  ADC1_PrescalerConfig(ADC1_PRESSEL_FCPU_D18);

  ADC1_Cmd(ENABLE);

  ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE);

  ADC1_StartConversion();

 INTERRUPT_HANDLER(ADC1_IRQHandler, 22)

 {

    /* In order to detect unexpected events during development,

       it is recommended to set a breakpoint on the following instruction.

    */

    //  ADC Conversion completed interrupt handler.

   

    u16 ADC_Raw_Value;

    static u16 ADC_dIntegrator=0;

    static u16 ADC_itIntegrator=0;

    static u8 ADC_mCount=0;

    

    ADC1->CSR &= ~ADC1_CSR_EOC;            //  Indicate that ADC conversion is complete.       

    ADC_Raw_Value = ADC1->DRH;            //  Read Most Significant bits first 

    ADC_Raw_Value <<= 2;                  //  Switch 2 bit to left(D9-D2)

    ADC_Raw_Value |= (ADC1->DRL & 0x03);    //  Add most and least significant bits 

    ADC_mCount++;

    ADC_itIntegrator+= ADC_Raw_Value;

    if(ADC_mCount == 20)

    {

      ADC_dIntegrator=ADC_itIntegrator ;

      callbackADC_Integrator(ADC_dIntegrator);

      DALIslave_SetAdcDataReadyFlag(TRUE);

      ADC_dIntegrator = 0;

      ADC_mCount = 0;           

    }

 }

void callbackADC_Integrator(u16 itADC_Integrator)

{

  ADC_Integrator = itADC_Integrator;

}

void DALIslave_SetAdcDataReadyFlag(bool state)

{

  AdcDataReadyFlag = state;

}

bool DALIslave_GetAdcDataReadyFlag(void)

{

  return AdcDataReadyFlag;

}

void DALIslave_AvgADCValue()

{

  static u8 AdcChannel = 0;

  u16 ADC_final;

  u8 ADC_low;

  u8 ADC_high;

  

  if (AdcChannel == 0)

  {

    ADC1->CR1 &= ~ADC1_CR1_ADON;                          //disable ADC conversion channel-0

    ADC1->CSR |= ADC1_CHANNEL_2;

    ADC1->CR1 |= ADC1_CR1_ADON;                           //start ADC conversion channel-2

    AdcChannel++;                                            //set to channel-2(current)

   

    ADC_temperature = ADC_Integrator / 20;                //get temperature average    

    ADC_final = (ADC_temperature );//* 33) / 10;

    ADC_low = (u8)(ADC_final & 0xff);           

    ADC_high =(u8)((ADC_final >> 8 )& 0xff);

    DALIP_SetTemperature(ADC_high, ADC_low);              //set temperature to RAM

  }

  

  else if (AdcChannel == 1)

  {

    ADC1->CR1 &= ~ADC1_CR1_ADON;                          //disable ADC conversion channel-2

    ADC1->CSR |= ADC1_CHANNEL_3;                          //set to channel-3(voltage)

    ADC1->CR1 |= ADC1_CR1_ADON;                           //start ADC conversion channel-3

    AdcChannel++;

    

    ADC_current = ADC_Integrator / 20;                    //get current average   

    ADC_final = (ADC_current );//* 33) / 10;

    ADC_low = (u8)(ADC_final & 0xff);

    ADC_high = (u8)((ADC_final >> 8 )& 0xff);

    DALIP_SetCurrent(ADC_high, ADC_low);                  //set current to RAM 

  }

  

  else

  {

    ADC1->CR1 &= ~ADC1_CR1_ADON;                          //disable ADC conversion channel-3    

    ADC1->CSR |= ADC1_CHANNEL_0;

    ADC1->CR1 |= ADC1_CR1_ADON;                           //set to channel-0(temperature)

    AdcChannel = 0;

    

    ADC_voltage = ADC_Integrator / 20;                    //get voltage average

    ADC_final = (ADC_voltage );//* 33) / 10;

    ADC_low = (u8)(ADC_final & 0xff);

    ADC_high =(u8)((ADC_final >> 8 )& 0xff);

    DALIP_SetVoltage(ADC_high, ADC_low);                  //set temperature to RAM

  }

  AdcDataReadyFlag = FALSE;

}

void main(void)

{

  while(1)

     if (DALIslave_GetAdcDataReadyFlag() == TRUE)

     {

       DALIslave_AvgADCValue();

     }  

}

  

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0