cancel
Showing results for 
Search instead for 
Did you mean: 

uart communication

vivekkaushik03
Associate
Posted on January 18, 2012 at 15:09

i want to communicate between two stm 8s discovery boards one will send the data through uart to the other one which will first receive the data and then transmit it to the real term using uart what are the necessary steps needed for this i am having problem in displaying the received data ,i am not been able to write a code for this,whether i have to do this in interrupt service routine or should check some flag and write the code in main function....any help will be apprecaited

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0