cancel
Showing results for 
Search instead for 
Did you mean: 

STM8S207 BootLoaer Iar

lee_lxw
Associate
Posted on October 16, 2014 at 18:16

 

 

 

Description:

 

 

 

In the STM8S For IAR Embedded WorkBench

 

I consulted AN2659 - AIP write the BootLoader, In the STM8S003F3,STM8S903K3 and 005 can be normal operation.

 

But in the STM8S207K6

 

 

First:

 

 

The sample program:

 

/****************************************************************************************/

 

// When shake hands with PC successfully.

 

CLK->CKDIVR = 0x00; // CLK Config

 

FLASH->PUKR = 0x56; // UNLOCK

 

FLASH->PUKR = 0xAE;

 

FLASH->DUKR = 0xAE;

 

FLASH->DUKR = 0x56;

 

RoutinesInRAM = 1; // Just a Flag

 

 

for(unsigned char i = 0;i < 248 ;i++) // Clear Flah for Program my Protect2

 

{

 

Write_Flah_Block_Data((0x8400 + 128*i),(unsigned char *)&Receive_Data_Buffer[0],128); //

 

Dead Here

 

}

 

// Mean I can not Program in the ram

 

 

// Program In the RAM

 

void Write_Flah_Block_Data(unsigned short Start_Address,unsigned char *Ptr,unsigned char Length)@''FLASH_CODE''

 

{

 

FLASH->CR2 |= 0X01;

 

FLASH->NCR2 &= (unsigned char)~0X01;

 

for( unsigned char i = 0; i < Length ;i++)

 

{

 

*(( PointerAttr unsigned char*) (unsigned short)Start_Address + i) = *Ptr;

 

Ptr++;

 

}

 

}

 

/*****************************************************************************************************************/

 

 

 

Second:

 

 

The ICF File

:

 

//

 

/////////////////////////////////////////////////////////////////

 

 

define memory with size = 16M;

 

 

define region TinyData = [from 0x00 to 0xFF];

 

 

define region NearData = [from 0x0000 to 0x17FF];

 

 

define region Eeprom = [from 0x4000 to 0x43FF];

 

 

define region BootROM = [from 0x6000 to 0x67FF];

 

 

define region NearFuncCode = [from 0x8000 to 0xFFFF];

 

 

define region FarFuncCode = [from 0x8000 to 0xFFFF];

 

 

define region HugeFuncCode = [from 0x8000 to 0xFFFF];

 

 

 

/////////////////////////////////////////////////////////////////

 

 

define block CSTACK with size = _CSTACK_SIZE {};

 

 

define block HEAP with size = _HEAP_SIZE {};

 

 

define block INTVEC with size = 0x80 { ro section .intvec };

 

 

initialize by copy { rw,

 

ro section .tiny.rodata,

 

section FLASH_CODE};

 

 

do not initialize { section .vregs };

 

do not initialize { section .*.noinit };

 

 

// Placement

 

place at start of TinyData { rw section .vregs };

 

place in TinyData { rw section .tiny.* };

 

 

place at end of NearData { block CSTACK };

 

place in NearData { ro section FLASH_CODE,

 

block HEAP,

 

rw }; // includes rw section .near.*

 

 

place at start of NearFuncCode { block INTVEC };

 

place in NearFuncCode { ro section .far.data_init,

 

ro section .huge.data_init,

 

ro }; // includes ro section .near_func.*

 

 

place in FarFuncCode { ro section .far.*,

 

ro section .far_func.* };

 

 

place in HugeFuncCode { ro section .huge.*,

 

ro section .huge_func.* };

 

 

place in Eeprom { section .eeprom.* };

 

 

 

 

Severity:

 

 

 

Medium

 

Due Date:

 

 

 

 

 

 

Product Type:

 

All

Project Name:

 

 

 

All

Production Forecast:

 

 

 

0

ku

 

 

(None)

Production Start Date:

 

 

 

 

 

(None)

 

Application Type:

 

 

 

(None)

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0