cancel
Showing results for 
Search instead for 
Did you mean: 

stm8s003f3 adc

n23
Associate II
Posted on May 11, 2015 at 22:03

Hello everyone

I am new to this forum, so hello. I am alsonew to STM en C. I am trying to learn everything step by step but get the stuck on the adc. I am trying to get the adc working on stm8s003f3 with the following code in STVD with Cosmic, and send the result to the pc using UART. Can anybode tell my what i am doing wrong? adc_value is 1010 from ADXL Same setup on arduino gives a reading somewhere around Any suggestion is welkom... Already thanks

/* Includes ------------------------------------------------------------------*/
#include ''stm8s.h''
#include ''stdio.h''
#ifdef _RAISONANCE_
#define PUTCHAR_PROTOTYPE int putchar (char c)
#define GETCHAR_PROTOTYPE int getchar (void)
#elif defined (_COSMIC_)
#define PUTCHAR_PROTOTYPE char putchar (char c)
#define GETCHAR_PROTOTYPE char getchar (void)
#else /* _IAR_ */
#define PUTCHAR_PROTOTYPE int putchar (int c)
#define GETCHAR_PROTOTYPE int getchar (void)
#endif /* _RAISONANCE_ */
int i;
int nCount = 0;
int adc_value = 0;
int adc_h = 0;
int adc_l = 0;
int nAdc_Buffer[10] = {0,0,0,0,0,0,0,0,0,0};
int nAdc_Hold = 0;
void main(void)
{
char ans;
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
UART1_DeInit();
UART1_Init((uint32_t)115200, UART1_WORDLENGTH_8D, UART1_STOPBITS_1, UART1_PARITY_NO,
UART1_SYNCMODE_CLOCK_DISABLE, UART1_MODE_TXRX_ENABLE);
/* ADC 1 Configuration ----------------------------------------*/
GPIO_Init(GPIOD, GPIO_PIN_2, GPIO_MODE_IN_FL_NO_IT );
ADC1_DeInit();
ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_0, ADC1_PRESSEL_FCPU_D2, ADC1_EXTTRIG_TIM,DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL0, DISABLE );
ADC1_StartConversion();
while (1)
{
for(i=0;i<20000;i++) // A delay loop
{
nop();
}
for ( nCount = 0; nCount< 10; nCount++){
nAdc_Buffer[nCount] = ADC1_GetConversionValue();
nAdc_Hold += nAdc_Buffer[nCount];
}
nAdc_Buffer[0] = nAdc_Hold / 10;
adc_value = nAdc_Buffer[0];
for ( nCount = 0; nCount< 10; nCount++){
nAdc_Buffer[nCount] = 0;
}
nAdc_Hold = 0;
printf('' %d\n'',adc_value);
printf(''adc value\n\r'');
}
}
PUTCHAR_PROTOTYPE
{
/* Write a character to the UART1 */
UART1_SendData8(c);
/* Loop until the end of transmission */
while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET);
return (c);
}
GETCHAR_PROTOTYPE
{
#ifdef _COSMIC_
char c = 0;
#else
int c = 0;
#endif
/* Loop until the Read data register flag is SET */
while (UART1_GetFlagStatus(UART1_FLAG_RXNE) == RESET);
c = UART1_ReceiveData8();
return (c);
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{ 
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif

#stm8 #adc
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
n23
Associate II
Posted on May 13, 2015 at 14:36

Maybe there is somebody who want to share a sample code for the adc? Or give me any suggestion how to get the ADC1 on de chip working?

Already thanks, Nick
Rita Jonkute
Associate II
Posted on November 16, 2017 at 11:56

Check if pin2 is actually channel0. check what happens if you put its actual channel name