cancel
Showing results for 
Search instead for 
Did you mean: 

STM8L152C6T6 USART1 interrupt probelm

sushil
Associate II
Posted on January 12, 2015 at 13:48

Hi , i am unable to transfer and receive data from usart1 using interrupt. I used polling method to transfer and receive data from usart1 and it is working OK. ( Tx and Rx are Shorted)

I am using STVD and Cosmic compiler to run the codes. My problem is that , with the below codes when i used enableinterrupt(); function , control is stuck somewhere and it not return to main loop .

So can you please tell us where is the problem. Also i am not able to run any interrupts too.

Codes are

main()

{

disableInterrupts();

DeInitClock();

DeInitGPIO();

/* Select HSI as system clock source */

#ifdef USE_HSI

CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSI);

CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1);

#else

CLK_SYSCLKSourceSwitchCmd(ENABLE);

/* Select 2MHz HSE as system clock source */

CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSE);

CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_4);

CLK_HSICmd(DISABLE);

#endif

UART_PORT_PIN_HIGH();

USART_Cmd(USART1,ENABLE);

 USART_DeInit(USART1); 

 CLK_PeripheralClockConfig(CLK_Peripheral_USART1, ENABLE);  

 USART_Init(USART1,BaudRate,USART_WordLength_8b,USART_StopBits_1,USART_Parity_No,USART_Mode_Tx|USART_Mode_Rx); 

 USART_ClockInit(USART1,USART_Clock_Enable,USART_CPOL_Low, USART_CPHA_1Edge,USART_LastBit_Disable); 

 USART_ReceiverWakeUpCmd(USART1,SET);

 USART_ITConfig(USART1,USART_IT_RXNE|USART_IT_TXE,ENABLE); 

 enableInterrupts();

USART_Tx_Buffer(''t'');

}

and in Interrupt handler file codes is below to write 1 in he lcd if interrupt executes.

  */

INTERRUPT_HANDLER(USART1_RX_IRQHandler,28)

{

/* In order to detect unexpected events during development,

   it is recommended to set a breakpoint on the following instruction.

*/

  //while (1);

gotoxy_lcd(1,2);

  LCD_WRITE(''1 '');

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0