cancel
Showing results for 
Search instead for 
Did you mean: 

STM8 Analog voltage stress

abelmeg2
Associate
Posted on March 23, 2010 at 12:49

STM8 Analog voltage stress

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
will2
Associate II
Posted on May 17, 2011 at 15:07

I don't think your Vref- pin can be brought low enough to sample -1 VDC.  (spec sheet says Vref- min is = Vssa).  You may have to level shift your signal until your low end is 0 V, which would make your range 0 - 7 V.  The absolute max for Vref+ is = Vdd, which is 6.5 V, so it would seem like you would also need to scale down your signal using something as simple as a 2-resistor voltage divider.