cancel
Showing results for 
Search instead for 
Did you mean: 

startup error for 12-pole BLDC motor

alevinthal
Associate II
Posted on March 23, 2010 at 17:24

startup error for 12-pole BLDC motor

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
alevinthal
Associate II
Posted on May 17, 2011 at 15:07

No. As stated in the post, it is STARTUP FAILED. 

 I have read App note AN1276 and the issue does appears to be in the alignment ramp and startup ramp table. How can I compute the correct parameter/table values for these functions? What other parameters must I set to get the system working? 

abelmeg2
Associate
Posted on May 17, 2011 at 15:07

Is the fault condition Overcurrent?

alevinthal
Associate II
Posted on May 17, 2011 at 15:07

I received a spreadsheet from ST online support that computes a startup ramp based on PWM freq, pole pairs, and rotational speed (rpm/s). I was able to install the new table in the code and now the motor runs fine.