cancel
Showing results for 
Search instead for 
Did you mean: 

SPI slave communication

ttran
Associate
Posted on September 21, 2011 at 00:02

Hi all,

I am working a project that has a SPI master on an OMAP-L138.  I had the four lines manually wired across from the OMAP-L138 to the STM8-S discovery board.  The connections are below:

OMAP SPI CS -> STM8 SPI NSS

OMAP SPI SCLK -> STM8 SPI CLK

OMAP SPI MOSI -> STM8 SPI MOSI

OMAP SPi MISO -> STM8 SPI MISO

This is my initialization function of the SPI as a slave.

 static void enable_spi_slave(void)

{

SPI_DeInit();

SPI_Init(SPI_FIRSTBIT_MSB, 

    SPI_BAUDRATEPRESCALER_8, 

    SPI_MODE_SLAVE, 

    SPI_CLOCKPOLARITY_LOW, 

    SPI_CLOCKPHASE_1EDGE,

    SPI_DATADIRECTION_2LINES_FULLDUPLEX,

    SPI_NSS_HARD,

    0x07);

SPI_Cmd(ENABLE);

}

 void main(void)

{

u8 command;

u8 *ptr;

enable_spi_slave();

while(1) {

u8 i=0;

//read_power_amp_status();

//update_ready_status_for_arm();

//while((GPIOE->IDR & 0x20) == 0x00);

if(SPI_GetFlagStatus(SPI_FLAG_RXNE) == SET) {

command = SPI_ReceiveData();

switch(command) {

case PTT_POWER_AMP_GET_STATUS:

{

/*

Write the statuses back to the SPI master.

*/

//for(i=0; i<27; i++) SPI_ReceiveData();

//SPI_ReceiveData();

bufptr = buffer;

for(i=0; i<12; i++) {

//while(SPI_GetFlagStatus(SPI_FLAG_TXE) != SET) 

while((GPIOE->IDR &0x20) == 0x00) 

{

if((SPI->SR & SPI_FLAG_TXE) == SPI_FLAG_TXE) {

SPI->DR = (u8)0x0d;

SPI->DR = (u8)buffer[i];

//SPI_SendData(buffer[i]);

//bufptr++;

}

}

//SPI_ReceiveData();

}

//SPI_SendData(0x00);

SPI_ReceiveData();

}

break;

default:

{

while((GPIOE->IDR &0x20) == 00) ;

SPI_ReceiveData();

}

break;

}

}

//delay(50);

  }

}

Basically, on the OMAP side I send over 0x1 followed by 12 zeros.  I can see that the 0x1 came over the wire on MOSI, which is my command (PTT_POWER_AMP_GET_STATUS).  I want to write back 12 bytes and that is main problem.  I constantly received 0x3a or 0x38.  What i sent back is 0xd 0xe 0xa 0xd repeated 3 times.  And on the scope, the signal for MISO is not what I expect.  Has anyone seen this problem using the SPI slave on the STM8 Discovery?

Any advice or comments is appreciated.

Thanks,

Tom

#stm8s-discovery
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0