cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with STM8LF3U6ATR, timer input capture mode

ashvinkumar
Associate
Posted on July 05, 2012 at 12:33

 

problem with STM8lF3U6ATR, timer input capture mode

dear sir ,

           I am configuring timer 2 in input capture mode for LSI frequency measurement, settings as per RM0013 doc. as per concept when 1st capture occures at (rising edge) ,whatever counter values (TIM2_CTRH, TIM2_CTRL) are loaded in TIM2_CCR1H,and TIM2_CCR1L at this interrupt event, 

          and when 2nd capture occure(rising edge) then also whatever incremented couter values (TIM2_CTRH,TIM2_CTRL) gets loaded in to the(TIM2_CCR1H,TIM2_CCR1L) , then as per formulae

            lsi_freq=(after N events capture occures)*Fmaster/difference of couter values loaded in TIM2_CCR1H,TIM2_CCR1L 

 but as per doc RM0013 i am not getting the results. counter values are not loading in to TIM2_CCR1L and TIM2_CCR1H, so i am in deep trouble ! 

     i am kindly requesting you all to please share your experience with me! 

also i am directly reading TIM2_CTRH,TIM2_CRTL at interrupt event then as per RM0013, but LSI frequency is comming at arround 17k-21k range for room temp. , but it is quantradectory with doc.

thanking you!

thanks and regards,

Ashvinkumar A Bhagat

(Embedded softwere developer) 
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0