cancel
Showing results for 
Search instead for 
Did you mean: 

LCD registers doesn't updated properly after wake up from active-halt mode in STM8L152R6 and STM8L052C6

hakanuckus
Associate

I am using STM8L152R6T6 and STM8L052C6 for my project.

The code wakes up from active-halt mode by RTC wake up interrupt. There is some LCD display memory (LCD_RAM) updates in RTC wake up interrupt routine.

The CPU executes this update function and some other functions. And after goes to active-halt mode again.

Although the CPU executes update function, there is not any change on display or LCD registers when i look in debug.

If I reduce system clock speed by using clock divider, problem doesn't occured. And also, when I added to code some dummy delay, this is solving the problem. BTW, I am using HSI (16 MHz)

I want to solve this problem officially, not by putting dummy delay to the code or reduce system clock speed. For instance wait for a flag.

Do you have any idea, or solution about this problem?

You can see and analyze the demo code in attachment.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0