issue with stm8s207rbt6 and eeprom
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-07-24 6:13 AM
Posted on July 24, 2012 at 15:13
Hi,
I'm using stm8s library 1.1.1.Cosmic C 4.2.10 Compiler.the mcu is stm8s207rbt6 I'm experiencing an issue writing a byte in the data eeprom while I'm receiving data on the uart3 (tried also on the uart1 and it's the same) The issue is that I get an unexpected reset of the mcu. I checked all the reset sources flags. and no one is set.. it seems just a reset without a precise reason. I found a workaround but is not ok for the my application. I have to disable the usart3 rx interrupt using (UART3_IT_RXNE_OR,DISABLE) after every reception and during the intervall I can write inside of the data eeprom without problems.. All the gpio are configured correctly ,Is really strange.. Do you have any suggestion ? thanks Spectre
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0