cancel
Showing results for 
Search instead for 
Did you mean: 

Is 5 microseconds the minimum resolution for the timers?

derek239955
Associate
Posted on February 04, 2013 at 22:44

I've tried both the 16 MHz HSI and 24 MHz HSE with the STM8/128-EVAL board, and I can only divide TIM4 down to an approximate 5-microsecond tick resolution.

Is this correct?

The settings I'm using with the 24 MHz HSE are TIM4_PRESCALER_2 (for a 12 MHz clock) and a TIM4_PERIOD of 11.

This should provide a 1-microsecond tick:

(11 + 1) / 12,000,000 = 1 usec.

But it seems to bottom out at approximately 5 microseconds.

I've also set Flash_Wait_States = 1 in the Debug Instrument > MCU configuration > Options window.

Any help would be much appreciated.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0