cancel
Showing results for 
Search instead for 
Did you mean: 

How start learning of stm8S003f3 ?

kalpeshpatil102
Associate III
Posted on February 26, 2018 at 12:00

hi  i am kalpesh  , i new in stm8 . I want to learn how to program in stm8. Please tell me which software should i use?

please help me . i have Stm8s003f3 20pin IC . 

i search @ internet i didn't  get ? 

please help me?

sorry for poor english

thank you

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Philipp Krause
Senior III
Posted on February 26, 2018 at 20:52

Here are two simple tutorials for the STM8S003F3:

http://colecovision.eu/stm8/STM8%20Min%20Sys%20Dev%20LED.shtml

 

http://colecovision.eu/stm8/STM8%20Min%20Sys%20Dev%20Serial.shtml

 

Both use SDCC for the compiler.

Philipp

Diego Moreno
Associate II
Posted on March 28, 2018 at 16:31

Take a look at this simple example that blinks the LED in the STM8S-DISCOVERY board using Timer TIM1. The code is written for a different MCU (STM8S105C6), but it is easy to port to STM8S003F3. You could use IAR or COSMIC+STVD as IDE. There are links on the GitHub README file and the code is ported for both.

https://github.com/diegomendesmoreno/STM8S_pisca_led_timer

 
kalpeshpatil102
Associate III
Posted on May 14, 2018 at 12:30

thank you . i will go through it. 

LOKESH VASHISHTH
Associate II
Posted on May 19, 2018 at 08:06

Hi 

I am lokesh.

kalpesh use IAR id for stm8.

very simple ,easy to use, easy for debugging.

IAR provide free version for 8kb memory limit.

i also attach a youtube channel link .

which provide all pheripheral video like gpio toggle , timer , external interrupt and etc.

https://www.youtube.com/channel/UCMnrf_QCcGwOv_TdvHxtTQQ/playlists