cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO problem

mmaana
Associate II
Posted on August 30, 2010 at 14:38

Hello! I have STM8S-Discovery, STVD+Cosmic_32K. I write:

 #include ''stm8s.h''

main()

{

 GPIO_DeInit(GPIOD);

 GPIO_Init(GPIOD, GPIO_PIN_0, GPIO_MODE_OUT_PP_LOW_FAST);

 TIM3_DeInit();

 TIM3_TimeBaseInit(TIM3_PRESCALER_2, 999);

TIM3_Cmd(ENABLE);

for(;;)

 {

if (TIM3_GetCounter() < 500) {

GPIO_WriteLow(GPIOD, GPIO_PIN_0);

 }

else {

GPIO_WriteHigh(GPIOD, GPIO_PIN_0);

}

}

}

All is normal, the light-emitting diode is shone, since the period of repetition 1 �?ºHz, but the problem what when I look an oscillograph on PD0 at that time when there should be a low level in its middle periodically appears a positive impulse??? Why?? Thanks!
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
lowpowermcu
Associate II
Posted on August 31, 2010 at 12:40

Hi petrd,

Why you don't use TIM3 in output compare mode, you can configure the duty cycle and you will get your timer controlling the led while the CPU is free.

NB: I have run your code on another device (i don't have discovery kit) but I couldn't reproduce the behavior you described.

good luck and regards,

MCU Lüfter