cancel
Showing results for 
Search instead for 
Did you mean: 

Does COSMIC support Little Endian approach ?

jeffrey23
Associate II
Posted on May 22, 2010 at 13:00

Does COSMIC support Little Endian approach ?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
swhite2
Associate III
Posted on May 17, 2011 at 15:08

(Post deleted)

jeffrey23
Associate II
Posted on May 17, 2011 at 15:08

After doing some experiment, I found that the COSMIC compiler supports the BIG endian approach for STM8S103F3 as default mode. Can it support Little Endian approach ?

swhite2
Associate III
Posted on May 17, 2011 at 15:08

Why do you care? If you had external peripherals on a bus I could understand but the STM8S103F3 doesn't have an external bus.

If you need to send/receive data in big-endian order

http://www.codeproject.com/kb/cpp/endianness.aspx

to perform the conversion. That's what people have been doing on PC's (80x86's are little-endian) for decades.

http://www.codeproject.com/kb/cpp/endianness.aspx

luca239955_stm1_st
Senior II
Posted on May 17, 2011 at 15:08

Hello,

in addition to the considerations above, it is interesting to underline that, for a micro like stm8, who is capable of multibyte operations (ld.w), the endianness is forced by the micro itself (-> does not depend on the compiler): STM8 is little endian.

Regards,

Luca (Cosmic)