cancel
Showing results for 
Search instead for 
Did you mean: 

Discovery vs ST-LINK

anickol
Associate II
Posted on August 03, 2010 at 08:19

Hello.

I've read on another forum that the Discovery board has the incomplete version of

ST-LINK that can program only s105c6 and nothing else via SWIM.

Please confirm or deny this information. Can Discovery be used for programming STM8L and other STM8S controllers ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Grom
ST Employee
Posted on August 03, 2010 at 14:21

Hello ,

With this embeded version of STLink you are ablle to program all STM8 devices (S,L & A). The only limitation is with voltage level for STM8L devices .

No voltage adapter has been added in this version so 1.8V is not supported.

STM32 devices are not supported.

Best Regards

Grom