cancel
Showing results for 
Search instead for 
Did you mean: 

Deviation in AWU clock frequency

wolfgang239955_stm1_st
Associate II
Posted on August 07, 2013 at 11:41

I'm using the BEEP function of my STM8S105, but it doesn't work as expectet. 

It's not that I need the exact frequency, but I want to know, why it

differs from the correct vallue, when chosing HSE as timebase.

Basic settings:

- external quartz crystal 16MHz

- MCU options:

   EXTCLK: External Oscillator (OPT4 EXTCLK = 0)

   PRSC: 16MHz to 128kHz (OPT4 PRSC[1:0] = 00)

- BEEP_CSR = 0xCE

1st test:

 option CKAWUSEL:

High Speed External

(OPT4 CKAWUSEL = 0)

-> expected fBEEP: 4kHz; real result: 2.69kHz

:

o

(

    ????

2nd test:

- option  CKAWUSEL:

Low Speed Internal

(OPT4 CKAWUSEL = 1)

-> expected fBEEP: 4kHz; real result: 4.09kHz

:

o

)

Any clue???

TIA,

WoRo

#beep #ckawusel #lsi
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0