cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in UART1_GetITStatus() of peripheral library 2.0.0

jheilig999
Associate II
Posted on July 11, 2012 at 19:00

According to what is documented on declaration of UART1_IT_TypeDef in file stm8s_uart1.h

it seems the function UART1_GetITStatus() calculate a wrong mask for the IT flags.

The UART1_IT_TypeDef says the lables were declared as ZYX, but the function uses Y and X swapped for their original meaning.

Changing the function as below makes things working:

ITStatus UART1_GetITStatus(UART1_IT_TypeDef UART1_IT)

 

{

 

    uint8_t itposSR = 0;

 

    uint8_t itposCR2 = 0;

 

 

    /* Check parameters */

 

    assert_param(IS_UART1_GET_IT_OK(UART1_IT));

 

 

    /* Get the UART1 IT index mainly for CR2 */

 

    itposCR2 = (uint8_t)((uint8_t)1 << (uint8_t)(UART1_IT & 0x0F));

 

    /* Get the UART1 IT index mainly for SR */

 

    itposSR =  (uint8_t)((uint8_t)1 << (uint8_t)((uint8_t)(UART1_IT & 0xF0) >> (uint8_t)4));

 

 

 

    /* Check the status of the specified UART1 pending bit*/

 

    if (UART1_IT == UART1_IT_PE)

 

    {

 

        /* Check the status of the specified UART1 interrupt*/

 

 

        if (((UART1->SR & itposSR) != (uint8_t)0x00) && ((uint8_t)UART1->CR1 & itposCR2))

 

        {

 

            /* Interrupt occurred*/

 

            return SET;

 

        }

 

        else

 

        {

 

            /* Interrupt not occurred*/

 

            return RESET;

 

        }

 

    }

 

 

    else if (UART1_IT == UART1_IT_LBDF)

 

    {

 

        /* Check the status of the specified UART1 interrupt*/

 

        if (((UART1->CR4 & itposSR) != (uint8_t)0x00) && ((uint8_t)UART1->CR4 & itposCR2))

 

        {

 

            /* Interrupt occurred*/

 

            return SET;

 

        }

 

        else

 

        {

 

            /* Interrupt not occurred*/

 

            return RESET;

 

        }

 

    }

 

    else

 

    {

 

        /* Check the status of the specified UART1 interrupt*/

 

        if (((UART1->SR & itposSR) != (uint8_t)0x00) && ((uint8_t)UART1->CR2 & itposCR2))

 

        {

 

            /* Interrupt occurred*/

 

            return SET;

 

        }

 

        else

 

        {

 

            /* Interrupt not occurred*/

 

            return RESET;

 

        }

 

    }

 

 

    /* Return the UART1_IT status*/

 

    return  RESET;

 

}

 

Functions for UART 2 & 3 could be affect by the bug too (I didn't check).

Bye

Giorgio

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0