2024-10-01 4:58 AM
Hello, I'm successfully using BSET and BRES assembler instructions where the position is constant. However, I'm having trouble getting it to work where the position is determined at runtime.
For example:
bset 0x500f, 2 ; works
ldw x, (0x03, sp)
bset 0x500f, x ; doesn't work
I've looked at several sites, but all seem to have constant positions.
One workaround would be to have a full list of BSET instructions, one for each position, and jump to the appropriate instruction based on a decision. This wouldn't be bad necessarily, but hoping for a better way.
References:
assembler instructions datasheet in PM0044, section 7 (specifically 7.4): https://www.st.com/content/ccc/resource/technical/document/programming_manual/43/24/13/9a/89/df/45/ed/CD00161709.pdf/files/CD00161709.pdf/jcr:content/translations/en.CD00161709.pdf
lujji's very helpful blog post: https://lujji.github.io/blog/mixing-c-and-assembly-on-stm8/
eforth: https://github.com/TG9541/stm8ef/wiki/STM8-eForth-Compiler-and-Assembly
a nice GitHub repo: https://github.com/search?q=repo%3Aaaw20904%2FSTM8_library%20bset&type=code
Solved! Go to Solution.
2024-10-17 2:24 AM
In fact, BSET, like all other bit operation instructions, can only be called with constants. There are two reasons for this: firstly, the instruction is executed in one cycle, which does not allow a variable to be fetched, and secondly, it only consists of 4 bytes, so there is no room for pointers.
Alternatively, you can also set bits in variables via the OR statement, but this increases the effort considerably because the variable must first be buffered in the accumulator and then moved back.
Regards
/Peter
2024-10-17 2:24 AM
In fact, BSET, like all other bit operation instructions, can only be called with constants. There are two reasons for this: firstly, the instruction is executed in one cycle, which does not allow a variable to be fetched, and secondly, it only consists of 4 bytes, so there is no room for pointers.
Alternatively, you can also set bits in variables via the OR statement, but this increases the effort considerably because the variable must first be buffered in the accumulator and then moved back.
Regards
/Peter
2024-10-17 3:43 PM
Thank you for the clarification. As a side note, since writing the question I've become more familiar with the PM0044 doc, where the details make it more clear that only constants are available.