cancel
Showing results for 
Search instead for 
Did you mean: 

bootloader stm8s

enoregrattoni
Associate
Posted on October 15, 2010 at 18:29

bootloader stm8s

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
enoregrattoni
Associate
Posted on May 17, 2011 at 15:11

I did some test to understand if bootloader start.

I set on one output and after two second I set off.

I see a delay of about 1 second at reset before to set on output if I set

055h  0aah in position 487e and 4880.

After the output set on and later off.

If I reset and immediatly run Pc program, I can see the character send by PC but I have

no answer from STM8S.

Seems also that i have to switch off to restart program.

PC program show message of timeout.

Waiting some tips