cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H74 microcontroller resetting while doing serial load using STM32 Cube Programmer V2.9 on few units

richaverma
Associate III

Hi,

  1. We are using STM32H74 microcontroller STM Bootloader ST Version 0x91.We are using STMCube Programmer V2.9 while during the serial programming using UART.
  2. On few of the units , we get the erase issue : Failed to erase memory . And then GETId not responded. All the power supply of the units are stable. On checking the NRST , it went low for around 30us . Refer attached.

richaverma_1-1751612982544.png

richaverma_0-1751612829455.png

On few good units , erase takes around 6.5seconds with V2.9 STM32Cube prograamer. 

This issue doesnt occur when we use STM32 Cube prograamer V2.19. Erase takes around 4.8seconds

On checking the difference between the two VERSIONS we found the command sent for erase is different in both the versions of STM32 Cube Programmer.

V2.9 sends command 0xffff00 data size :3 Bytes. This is a mass erase.

While V2.19 sends 0X0000000000 DATA size: 5bytes. It is a page wise erase. The erase time taken by V2.19  is less compared to V2.19.

Once the unit switches to the STM Bootloader, the IWDG timeout will be 16 seconds (32 kHz clock, pre-scaler set to 256 [Max Value] and window set to 2000). But on disabling this interrupt , we are able to do serial programming even with V2.9. Since the timeout for reset is 16 seconds , we are not able to understand how delay in erase using V2.9 can cause this reset.

Also , why it never happens when programmed with V2.19

richaverma_2-1751613817174.png 

richaverma_3-1751613870961.png 

richaverma_4-1751613942902.pngrichaverma_5-1751614049445.png

Please note on doing only Bank 1 ERASE with V2.9 there is no issue. issue happens only during Mass erase V2.9 STM32Cube programmer.

Programming & erase using JTAG has no issues.

Any leads will be appreciated.

 

10 REPLIES 10

Hi ,

Yes , this is not closed . Still awaiting more responses.

May be by mistake i accepted the answer as solution.