Skip to main content
Semer CHERNI
ST Employee
July 10, 2023
Question

STM32CubeMX 6.9.0 released

  • July 10, 2023
  • 1 reply
  • 1897 views

We are pleased to announce you that the official release of STM32CubeMX V6.9.0 is available for download here

  • What is new in STM32CubeMX V6.9.0?
    • Added the support for new microcontrollers in the STM32U5 series
    • Added the support for new microcontrollers in the STM32WBA series
    • Added the support for two new boards related to the STM32U5 series: STM32U5G9J-DK1 and STM32U5G9J-DK2
    • Added the support for one new board related to the STM32L4+ series: STEVAL-SMARTAG2
    • Added the support for the memory management tool for the STM32H5 and STM32U5 series
    • Added the support for new boot paths for the STM32H5 series
    • Added makefile generation in dual context for the STM32H7, STM32L5, and STM32U5 series
    • Added hierarchical project support in the Example Selector for the STM32U5 and STM32WL series
    • Added user authentication functionality
    • Added the support for processing before and after code generation
    • Upgraded the JDK11 to Adoptium™ Termurin™ 17.0.6
  • Main fixed issues
    • 121529 [Example selector] Management of hierarchical projects.
    • 130926 [Project generation] Makefile project type for dual-context projects is now supported.
    • 134482 [Boot path configuration] The boot path functionality now supports the Keil® IDE.
    • 144716 [Installer] Added the installation path in the PATH environment variable.
    • 145844 [CubeMX][ETH][LwIP] Bug in ethernetif.c file for Nucleo-F429ZI with ETH + LwIP(IPv6)
    • 147572 [STM32CubeMX] [SYS] Change in the implementation of stm32l4xx_hal_timebase_tim.c provoked run time issues
    • 150288 [MDMA] wrong channel number in the generated code
    • 151261 [U5]bug in initialization of GTZC, missing clock enable
  • Known issues fixed and problems and limitations
    • Please refer to the release note.
    This topic has been closed for replies.

    1 reply

    Explorer II
    May 30, 2024

    Can you please provide info on the feature "Added the support for processing before and after code generation"? I have not been able to find any documentation. This feature would be very useful to my team. I attempted to run a powershell script that writes a string to a file. I added this script as an 'after processing' step. The generation output indicates the script was run, but the script appeared to not have any effect.