STM32CubeMX (MPUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.12.0 released

We are pleased to announce you that the official release of STM32CubeMX V6.12.0 is available. What is new in STM32CubeMX V6.12.0?New MCUs/MPUs series : STM32WB0 ,STM32MP25XX and STM32C071XXAdd support new CPNs STM32G4: Add support STM32G4 'Z’ and STM...

Resolved! undefined reference to `HAL_ADC_Init'

I've been trying for hours to read an analog value from a pin and write it over UART with no success on my STM32MP1. I've assigned PF14 to ADC2_INN2 and set IN2 to "IN2 Differential", then I generate the code and when I try to build I get a bunch of ...

msche.1 by Associate III
  • 1666 Views
  • 5 replies
  • 0 kudos

STM32MP157C-DK2 - Can not enable UART8 in uboot?

Hi,We are trying to replace UART8 instead of UART4 in uboot and UART8 doesn't work for us.We change to UART3 it work just fine.When we open STM32CubeMX, hopefully we can find something, but seem the application doesn't allow us to select UART8.Anyone...

0693W00000aIwmdQAC.png
Dat Tran by Senior II
  • 391 Views
  • 0 replies
  • 0 kudos

Resolved! IPCC interrupt issue in stm32mp157A ?

Hello,We are using STM32MP157A.We are working on IPCC from A7-0,A7-1 to M4.We are getting IPCC interrupt A7-1 to M4,But when we are not getting interrupt from A7-0 to M4.In cubeMx it is showing NVIC to IPCC RX1 and TX1, but not showing to RX0,TX0.we ...

0693W00000Y8qf8QAB.png 0693W00000Y8qfSQAR.png
Srikanth1 by Associate III
  • 504 Views
  • 1 replies
  • 0 kudos

Resolved! Where a stm32mp1xx.h file?

I ran GENERATE-CODE on STM32CubeMX and M4 files were created. There is #include "stm32mp1xx.h" in stm32mp1xx_hal_def.h in Include, but there is no stm32mp1xx.h file. where is it?

安保.1 by Associate II
  • 409 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP157A, enable USART2 through ST-LINK

Hi,   I have a STM32MP157A-EV1 board. I'm running it in the engineering boot mode and programming the Cortex-M4 directly through the STM32CubeIDE. At the moment, I do not use the Cortex-A7.   I would like to enable USART2 and use it through the ST-LI...

0693W00000VOTVUQA5.png 0693W00000VOTVjQAP.png
Fnx_QT by Associate III
  • 706 Views
  • 4 replies
  • 0 kudos